Part Number: DS90C031 Other Parts Discussed in Thread: DS90C032 ,
Devices used: DS90C031, DS90C032 1. When the input to the LVDS driver was fed with a 5V,500 KHz clock signal, the DOUT+ line at the LVDS driver ouptut was seen as stuck at 1.2 V. At the same…
Part Number: DS90C031 Other Parts Discussed in Thread: DS90C032 , SN65LVDT14 Hello,
I am trying to communicate between two boards. One is using the DS90C031 and the other is using the SN65LVDT14. The RX device burnt up (actual burn mark) and failed when…
ds90lv032atm.ibs Hi Sakai-san,
It is not possible to create the DS90C032 spice model now. The best model to use is the IBIS DS90LV032A model attached.
Regards,
Lee
Part Number: DS90C032QML Other Parts Discussed in Thread: DS90C032 Hello Support,
We have had an LVDS receiver failure (this is not the first).
Investigation is ongoing, but the receiver is drawing 170 mA from its Vcc pin. The connection pair that was…
Hello Sandesh,
SN65LVDS387 is a standard compliant LVDS driver and it should work with any standard LVDS receiver, including DS90C032. Please provide a block diagram (or a simple sketch) showing what is connected to both sides of SN65LVDS387, the LVDS…
Part Number: DS90C031 Other Parts Discussed in Thread: DS90C032 , DS91M040 , SN65LVDS105 I want to use DS90C031 as LVDS driver and i will be connecting one output channel of driver to 4 receivers (Each using DS90C032), at a maximum distance of 2 meters with…
Other Parts Discussed in Thread: DS90C031 , DS90C032 , ADC128S102 We are developing a sensor system for use in terrestrial radiation environments. We do not require the intensive part tracking documentation of space products. Our application will not tolerate…
Hi Julian,
I think if this issue is causing the part to fail, it is not as much a common mode voltage range issue as it may be that the device is being thrown out of its absolute maximum rating. I do not think moving to another device with enhanced common…