Part Number: F28M36P63C2 Hi, support team
My customer needs a substitute of F28M36P63 I found a TMS320F28388DPTP with similar functions. But Inventory is also low.
Could you provide other substitute of F28M36P63 with better Inventory ?
Thanks so much. …
Part Number: F28M36P63C2 Hello,
Is there an excel sheet or matlab scipt that models the attached document "PR Controller mapped to 2p2z"?
Thanks,
Srini
Part Number: F28M36P63C2
Tool/software: Code Composer Studio
Hi TI
Since F28M36P63C2 controlCARD is no longer in production I need to find a replacement.
Right now I am using the ethernet connection to to communicate with LabVIEW and set parameters.
…
Part Number: F28M36P63C2 Team,
Several GPIOs support the input qualification feature, see datasheet chapter 5.9.6.2 GPIO - Input Timing. Is this feature available for GPIO21 when used as 'McBSP-A receive data' ? So that the McBSP input goes through…
Part Number: F28M36P63C2 Hello,
I am using the DDSRF pll function to estimate grid angle and use that theta subsequently in the generation of my inverter's three phase output. The frequency of my three phase output is matched with that of the grid frequenxy…
Part Number: F28M36P63C2 We're using TI Concerto microprocessor F28M36P63C2ZWT in a product. There are two GPIO pins (GPIO12, GPIO13) are used as external input to trigger events (falling edge) happening on the I/O. To filter out the noise, we implement…
Other Parts Discussed in Thread: TMS320F28379D , TMS320F28377D Hi Todd,
we are now starting a new development with C2838xD. It's a motor control application . We have also noticed with the new Code Composer Studio (version 10.2.0.00009) that TI-RTOS for…
Part Number: F28M36P63C2 Other Parts Discussed in Thread: UNIFLASH , C2000WARE
Hi,
We developed a controller board using a F28M36P63C2 chip, in which boot mode pins were assigned to BOOT_FROM_FLASH mode permanently. Besides, the only serial port connected…
Part Number: F28M36P63C2 Other Parts Discussed in Thread: DRV8312 , DRV8303 We’re using TI Concerto Microcontroller F28M36P63C2ZWTS22 to drive DRV8303 and DRV8312. The product has been launched last year and we have some failure issues
It has been…
Part Number: F28M36P63C2 Other Parts Discussed in Thread: C2000WARE
Dear all,
my customer thinks about using a webserver to update the firmware of both cores of an F28M36P63C2.
What do you think, is that possible. If yes, can somebody describe the procedure…