Part Number: FDC2114EVM Hi,
I had a problem while programming the FDC2114EVM using the EVM GUI firmware upgrade feature. While it was uploading, it was taking quite a while so I decided to close the application and restart the firmware upgrade. Doing…
Part Number: FDC2114EVM Other Parts Discussed in Thread: FDC2114 , Dear TI
Here are my questions:
How much capacity does "C sensormax" have?
And, please tell me how to calculate the "C sensormax".
Part Number: FDC2114EVM Other Parts Discussed in Thread: FDC2114 Hi! I am using FDC2114EVM to measure capacitance. I connected my own sensor to the channel. I have some questions.
i) I can see the change of capacitance, but comparing to the LCR meter…
Part Number: FDC2114EVM Hi, I am currently working on a water level sensing project where you won’t necessarily know when the water level is at its zero point. I am wondering how to get around this issue to calculate the level using the equations listed…
Part Number: FDC2114EVM I'm testing the FDC2114EVM using the EVM GUI. When i set the register of the drive current, I found the frequency changes with the drive current. This is normal? Where is my issue?
I used the singal channel,and control the…
Part Number: FDC2114EVM Other Parts Discussed in Thread: FDC2114 Hi, TI
Please tell me how to measure 105pF or more with FDC2114EVM.
With the current settings, I can only measure up to 105pF.
Please tell me how to measure 110 or more with this device
…
Part Number: FDC2114EVM Other Parts Discussed in Thread: LDC1314EVM , FDC2214 , FDC2114 , LDC1314 , Hi,
I own both FDC2114VM and LDC1314EVM and I would like to use them to evaluate my own hardware sensor board which is based on the FDC2214. I have separated…
Part Number: FDC2114EVM Other Parts Discussed in Thread: FDC2114 , Hi, TI
FDC2114EMV has 18μH inductor on the board.
When I want to measure 500pF~1500pF, what size inductor do I use?
And, when I use the optimal inductor to measure 500pF~1500pF, what are…
Part Number: FDC2114EVM Hello team,
My customer tried to download the GUI tool " Sensing Solutions EVM GUI Tool v1.10.0 " from TI.com, but can't access it with the error page as attached. Is there any way to get the software?
Thanks in advance…