Part Number: DRV5032-SOLAR-EVM Other Parts Discussed in Thread: DRV5032 , DRV5053 Dear Sirs, I receved your DRV5032 Ultra-Low Power, 1.65V to 5.5V Hall Effect Switch Sensor Evaluation Module but I’m not scure if it can be helpfull for me. I need to mesure…
Part Number: TPA6304-Q1 Other Parts Discussed in Thread: TAS5414 Gregg,
I think Adam Daluga (TI's customer-facing engineer for Indiana) and my boss have completed exchange of TI's NDA to cover this. I am in possession of a long form data sheet for the…
Part Number: XIO3130EVM Other Parts Discussed in Thread: XIO3130 Hello, Dear Owner
Does the XIO 3130 EVM kit also come with an ExpressCard adapter board? Or, do I need to purchase an ExpressCard adapter board separately?
-----------------------…
Other Parts Discussed in Thread: DRV8703-Q1 Thank you i will do accordingly application...
i have source code of DRV8703Q1 EVM (brushed motor controller and driver PCB) ( MSP430G2553IPW20 MICROCONTROLLER) which was downloaded from Ti website..
Now…
Part Number: TDA2HV Tool/software: Code Composer Studio Hi friends,
I have the J6 EVM board, and there is a JTAG interface in the EVM, but the XDS200 emulator is 20pin
how can I get the converter to trans the 20pin to mipi ?
Thanks a lot.
…
Other Parts Discussed in Thread: CONTROLSUITE , MOTORWARE , DRV8301-69M-KIT Folks,
I would like to implement a low-cost BLDC motor controller for mechatronics/robotics applications that combines the capabilities of the DRV8305N BoosterPack Eval Module…
Part Number: DAC34H84EVM The module, I bought( DAC34H84 EVM(Rev D), is not compatible mechanically with FMC-DAC adapter. It is impossible to connect boards to each other.
Are there many versions of the FMC-DAC adapter?
Part Number: TMS320C6678
Wasn't specifically on the forums because of this, but a post I just read raised a troubling concern.
Given lead times and whatnot, I'm using a couple of TMS320C6678 EVMs and was planning on inserting them into my Windows…
Part Number: USB-TO-GPIO Tool/software: Code Composer Studio Hello Sir,
Can I get the source code project for USB Interface Adapter in code composer studio IDE?
I have MSP430F5529 Iaunchpad and I want to use micro wire interface.
I also want to…
Other Parts Discussed in Thread: DRV8307EVM Hi,
My customer tries to operate motor with DRV8307EVM. They use the hall element. it is "HW-105W". VM=24V.
At this case, What are we select at JP3 and JP4? I think think that we select the following. Is…