Hello,
To add to this, we have some reference designs for keypads using our inductive sensing devices. Devices like the LDC3114 still use I2C but only need to be configured at startup and then can provide digital outputs for the button presses.
…
Part Number: DRV8363-Q1EVM I am currently working with the DRV8363-Q1EVM evaluation module and noticed that it requires external Hall sensors for sensored trapezoidal BLDC motor control. Could you please recommend suitable Hall sensors that are compatible…
Part Number: AM62P Hi, I am using latest sdk in my evm tisdk-default-image-am62pxx-evm-11.01.05.03.rootfs.wic.xz, I Have connected display using HDMI connector and I am able to see the ti-apps-launcher appilcation.
I have disable and stoped the ti-apps…
Hi Suren Porwar
Now I use TI_AM62pxx_HyperCluster-1920x720_demo-latest.7z and rebuild it in my 11.1 SDK sysroot , generate the newer binaries
there is build log , you can check it
Fullscreen
3480.build_log.txt
Download
[linux-devkit…
Hey Francois,
The DRV8363-Q1 EVM was built for compatibility with LAUNCHXL-F280049C. In one of our initial revisions we had challenge running HALL C to J9.17.
The Hall signal would not toggle which affected Hall based commutation. Therefore, We…
Hello Chase
Chase Jeong said: Could you check that how can I connect TQL50A to DRV411 EVM?
You would basically remove the connections of the hall sensor and compensation coil to our device. I assume you just want to use the hall sensor and compensation…
Part Number: MCT8316Z Hi, I'm using the MCT8316Z (spi version) BLDC motor controller, to control a brushless motor with digital hall effect sensors. My schematics (I believe) follows the EVM and reference designs, and is nothing out of the ordinary. I…
Hi Henry,
Thank you for your interest in the DRV8353R EVM.
You are correct, unfortunately this board only supplies 3.3V to the hall power.
The DRV8353 Device itself will work just fine with this motor, but unfortunately the board was designed without…
Hi
There is no errata or issue observed with PWM frequency.
How are the HALL sensors are connected? Can we verify the HALL type and biasing recommendation including noise filtering as per data sheet?
Are you testing it on EVM?
Please share motor…
Hello Liu Billy,
Can you please confirm you have reviewed the schematic using the below checklist. Please review the schematic using the checklist and share the updated excel with comments
AM62L Schematic checklist
https://e2e.ti.com/support/processors…