Part Number: HDC2010 Hello,
We are integrating the HDC2010YPAR temperature and humidity sensor into our design, but we have encountered an issue:
We can successfully read the temperature and the Manufacturer ID, as well as turn on the internal heater…
Part Number: HDC2010 Tool/software: Hi,
We use the HDC2010 for the t emperature and humidity collection,
and now, The SMT processing factory will first help us mount the hygrometer onto the PCB.
After returning, we will conduct random humidity measurement…
Part Number: HDC2010 Other Parts Discussed in Thread: HDC3020
Tool/software:
Hi Team,
Here are some questions about HDC2010. please help!
1. Can HDC2010 detect 0% RH? or just suit for 20~80%RH?
2. Any real case or customer use to detect 0…
Part Number: HDC2010 Tool/software: Hi, we are currently using the HDC2010 to monitor environmental temperature and humidity.
In our application, the presence of ammonia gas causes the HDC2010 humidity readings to become higher than expected.
For…
Part Number: HDC2010 Tool/software: Hi expert,
The humidity sensor selected is used in the environment of energy storage containers, with a temperature range of -40℃ to 85℃ and a humidity measurement range of 5% to 95% (at least 15% to 90% is required…
Part Number: HDC2010 Hi team,
What is the required keep-out clearance for the thermal pad around the HDC2010 sensor area?
Also, could you please provide a thermal pad design guide for our reference?
Thanks
Part Number: HDC2010 Other Parts Discussed in Thread: HDC3020 , HDC3022 Hi sir
we need a sensor for extreme environments-
1.
Please confirm whether this sensor (HDC2010YPAR) can operate correctly within the range of 500 feet below sea level to 20…
Part Number: HDC2010 Other Parts Discussed in Thread: HDC3021 , HDC2021 , HDC3022 , HDC2022 Tool/software: Hello TI Team,
I am evaluating the HDC2010YPAR humidity and temperature sensor for an environmental monitoring application that involves measuring…
Part Number: HDC2010 Tool/software: HI TI
My device uses HDC2010, but condensation always occurs on the device during use. Due to condensation, the pins of HDC2010 are short circuited.
May I ask how to waterproof HDC2010?
Can I apply conformal coating…
Part Number: HDC2010 Tool/software: At present, the design of our product mechanism is as shown in the diagram on the TI document, but there is a 1cm gap between the IC and the mechanism hole on our PCB. However, I refer to the TI design document and…