Part Number: HDC2010 Hi Sir,
Our customers reported that the temperature and humidity measured by HDC2010 has a large deviation. Comparing the value measured by the calibration instrument with the data directly monitored by HDC2010, it is found that…
Part Number: HDC2010 Hi expert,
My customer has question from the datasheet, there's a parameter called "IDDHEAT".
There's a description only mentioned that operating at -40~85 degree. But we are not able to understand this parameter is…
Part Number: HDC2010 Hi team,
When they read registers from 0x00 - 0x03, I think they need to set the slave address and also 0x00 as the pointer like Figure 3-1 and Figure 3-2 of the link as below. However, it seems that Figure 3-3 doesn't set 0x00 as the…
Part Number: HDC2010 Hi expert,
TI don't recommend rework HDC2010 from datasheet description 10.1.1.3 Rework.
Could you please give me your advice for the following cases?
1. If customer will find the assemble issue on HDC2010. They would like to…
Part Number: HDC2010 Other Parts Discussed in Thread: HDC3020 Hello,
I was wondering if the NIST traceability only applied to the temperature sensing component of this device or if it also meets NIST relative humidity tracing. I couldn't find anything…
Part Number: HDC2010 Hi,
when customer is testing HDC2010, they found it work at self-heating, temperature read as 70℃, it recover until reset IC.
Address 0x0E=0x50, "heater on" is off.
and the test environment is as below:
temp: around 55℃ …
Part Number: HDC2010 I'm using the HDC2010 installed on the BASSENSORS Booster Pack, on a Tiva TM4C board.
Through I2C I can set and read back all of the 2010's registers. I verified that the manufacturer ID and the part ID numbers are correct, too…
Part Number: HDC2010 Other Parts Discussed in Thread: HDC2022 hi:
Hdc2010 is used in IPx4 waterproof structure.
Because it is waterproof, it exists in closed space.
The air enters into the structure through waterproof and breathable membrane (IP54 standard…
Part Number: HDC2010 Other Parts Discussed in Thread: CC2640 Hello, we have the following issue when doing a measurement using HDC2010. The sequence is as follows:
1) Power on the sensor, wait 4.5 ms. (the datasheet says the sensor should be ready in at…
Part Number: HDC2010 Hi expert,
The datasheet is described about after reflow as below,
10.1.1.2 Soldering Reflow
For PCB assembly, standard reflow soldering ovens may be used. The HDC2010 uses the standard soldering profile IPC/JEDEC J-STD-020 with…