Part Number: HDC3020-Q1 Other Parts Discussed in Thread: HDC3020EVM , This post is regarding my previous inquiry: https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1624627/hdc3020-q1-significant-self-heating-observed-on-both-custom-pcb…
Part Number: HDC3020-Q1 Other Parts Discussed in Thread: HDC3020 , HDC3021 Dear Engineers
When assembling products using sensors such as the "HDC3020-Q1," how does the adhesive affect the sensor?
I'm considering using "ThreeBond 1225B," which is primarily…
Part Number: HDC3020-Q1 Other Parts Discussed in Thread: HDC3020EVM
Dear TI Team,
I am currently developing a high-volume production PCB using the HDC3020-Q1. Throughout several prototyping stages, I have observed that this sensor is highly sensitive…
Part Number: HDC3020-Q1 Hi,
I would like to use the HDC3020-Q1 to sense external Humidity
Im planning to attach it to a panel with a sealing rubber between the sensor and the panel
are there any guidelines to do it:
Pressure I can apply on the…
Part Number: HDC3020-Q1 Other Parts Discussed in Thread: HDC3020
Tool/software:
Team,
Customer enabled heater with command 0x306D. Read status through 0xF32D command and return 0x2000 bit 13=1 mean heater is enabled. The heater is configured as…
Part Number: HDC3020-Q1 Other Parts Discussed in Thread: HDC3020
Tool/software:
Team,
Customer environment 25C, 5%RH. Then they enable heater full power for 5 min. Temperature goes to 50C. Then sometimes, ALert is asserted and Status register…
Part Number: HDC3020-Q1 Dear Engineers
I recently asked about the effect of adhesives on sensors. (Request number: E2E1615574)
I have selected a new adhesive, and I would like to know if it is worth considering making a prototype.
Based on the ingredients…
Part Number: HDC3020-Q1 Other Parts Discussed in Thread: HDC3020 Tool/software: This customer built a batch of 200 boards. Some routing of the PCB happened after the boards were assembled which resulted in contamination of the polymer (these are parts…
Part Number: HDC3020-Q1 Other Parts Discussed in Thread: HDC3020 Tool/software: In trying to minimize the heat generated around the HDC3020-Q1, does it make sense to minimize I2C traffic? The application has the pullup resistors away from the cutout area…
Part Number: HDC3020-Q1 Other Parts Discussed in Thread: HDC3020
Tool/software:
Team,
Customer HDC3020 works fine already. They want to implement heater function for condensation remove now.
Customer enable heater with commander 0x30 0x6D run…