Part Number: INA209 Other Parts Discussed in Thread: SYSCONFIG , , INA226 Hi Experts,
Our customer is looking for the INA209AIPWR IBIS model urgently. Please share if available and can be shared with the customer. Thank you,
Best regards, Gerald
Part Number: INA209 Hello,
I'm using 10 x INA209 in my design.
F= 100KHz
I'm having problem of accessing the ones which are configured to I2C ADDR by strappin A1 A0 to SDA / SCL (for exampleL addr 0x42 (A1=GND, A0=SDA))
The DS says :
"The state…
Part Number: INA209 Hi,
Good Day. Customer would like to know the gain error value/formula when the input filter circuit is used. On the INA21X datasheet, there are gain error formulas but in the INA209 datasheet there are no gain error formulas. Please…
Part Number: INA209 Hello,
I am new to circuit design and I am having trouble finding information on how to program the behaviour of the GPIO pin on the INA209. All I need the device to do is to set the GPIO pin high once the input power reaches above…
Part Number: INA209 Other Parts Discussed in Thread: INA226 , INA231 , INA300 Hello,
This part measures shunt voltage to infer current and bus voltage. I am attempting to evaluate the measurement error across the input and voltage current range of my application…
Part Number: INA209
Hi Sir,
May I have your help to review INA209 relative SCH and layout?
EXUFS_VCCQ2_OUT2= 1.8 V
UFS_VCCQ2= 1.8 V
EXSDVCC_OUT2= 3.3 V
SD_VCC= 3.3 V
Thank you.
Best regards,
Edward Chen
Dear Dino,
Yes. It is due to the fact that at that point of operation, the common mode is now exceeding the supply voltage. Therefore, when this occurs, the part switches internally and, as a result, begins to draw additional current at the inputs of the…
Other Parts Discussed in Thread: INA209 Hello Team,
the INA209 supports the monitoring of the current via the internal Comparator + DAC beside the ability of measuring the current via an ADC.
Can you specify how fast it can be triggered the comparator…