Part Number: INA851-INPUT-OUTPUT-RANGE-DESIGN-CALC Other Parts Discussed in Thread: INA849
I am currently evaluating the INA849 instrumentation amplifier in simulation, and I am seeing an unexpected output value that does not match the theoretical calculation…
Hi Manikandan,
I'd recommend using the INA851-INPUT-OUTPUT-RANGE-DESIGN-CALC tool for quick verifications. I always do as it's super useful.
Your understanding of the device is correct. It's the input stage that would be clipping as shown below: …
Part Number: LM70XX0-CALC To whom it may concern,
In our design, we observed that increasing Rboot from 1ohm to 10ohm helped recude the peak voltage stress measured between SW and PGND. Howvever, since the datasheet recommends 1ohm, we would like…
Part Number: UCC25660X-CALC Other Parts Discussed in Thread: PMP23464 Hi,
I am designing a 500W Li-ion battery charger. Output voltage range is 30 to 50V with fixed 10A charge current. Seems that PMP23464 is a good reference. But I cannot found any…
Part Number: LM317 I'm trying to understand the lm317 datasheed where the input voltage is listed at 40 v, but there is this statement:
"The regulator is floating and detects only the input-to-output differential voltage. Thus, supplies of several hundred…
Part Number: TMUX1072 Dears,
TMUX1072 is selected to be used for switch RS485 signals. What about the Voltage range on analog input/output pins of NC1,NO1,NC2,NO2? From the attached datasheet, it says 5.5Vmax. If the Vcc is 3.3V, can those four pins…
Part Number: UC3845 Hi Team,
During the startup process of the flyback power supply, an overvoltage occurs at the transformer output.
Synchronously collecting the PWM output pin, after the overvoltage occurs, the negative feedback regulation of the…
Part Number: RC4558 Other Parts Discussed in Thread: RC4580 , Dear Technical Support Team,
Could you share the spec for Input range(VICR) and output range(VOUT ) for ±5V supply?
Datasheet has only ±5V version.
Best Regards,
ttd
Part Number: ADS5287 Hi TI Team,
We are interfacing the ADS5287 with an FPGA using the serial LVDS output and have a couple of questions regarding the ADC output format and analog input range.
1. ADC output showing 12 bits
The ADS5287 is specified…
Part Number: TLV9002-Q1 Other Parts Discussed in Thread: TLV9002 , AMC0311D-Q1 , Hi team,
My customer is using TLV9002 to converter differential output of AMC0311D-Q1 to single ended output . TLV9002-Q1 is using single rail power supply. When high voltage…