Part Number: ISO1044 Hi team
I want to know how to do iso1044 high voltage test method.
1,According to 9.2 Typical Application, how do I choose the voltage test site?
2,Please confirm the test specification: AC 8 kV/60s.
-RAIN
Part Number: ISO1044 Other Parts Discussed in Thread: ISO1042 , Hi team,
I’m trying to understand the distinction between ISO1044 and ISO1042‑Q1 CAN transceivers. On paper, both devices appear to have similar temperature ratings, yet ISO1042‑Q1 is designated…
Part Number: ISO1044 Other Parts Discussed in Thread: ISOW1044 , I am designing a small asset tracking device that includes 2 isolated CAN busses.
I do not have the room on the board for 2 ISOW1044 chips
I could use 2 ISO1044 chips however I dont…
Part Number: ISO1044 Tool/software: Hello TI team,
I am designing a CAN bus up to 100 m with about 10 nodes at different locations. Each node has its own local power supply.
I plan to use ISO1044 isolated CAN transceivers. To simplify the design,…
Part Number: ISO1044 Hi,
I started to use your isolated can bus transceiver and it works fine but I needed to replace it time to time cause during startup it burns, I used the recommendd protection in the data sheet but I still have this issue, It seems…
Part Number: ISO1044 Hi TI Team,
I am using the ISO1044BD isolated CAN transceiver in a multi-node CAN network and am facing an unexpected issue.
Network Topology
CAN Transceiver: ISO1044BD
Total Nodes: 10
Bus Topology: Linear CAN Bus
CAN…
Part Number: ISO1044 Tool/software: Dear Experts,
We use ISO1044 in isolated application but in one case we do not need isolation for CAN but since we use
ISO1044 everywhere we do not want to introduce a new CAN transceiver so my question is is…
Part Number: ISO1044 Tool/software: Hi Team,
The iso1044 has 3 different alternatives in the link ( https://www.ti.com/product/ISO1044 ) attached all with varying prices on the same 1ku quantity. Any differences between ISO1044BD, ISO1044BDG4 and ISO1044BDR…
Part Number: ISO1044 Tool/software: Hello,
The host MCU needs to communicate with 2 external CAN devices. These devices will NOT be on the same CAN bus. They will be on different bus that talks to the host MCU using two different CAN peripherals of…
Part Number: ISO1044 Other Parts Discussed in Thread: TCAN3404 Tool/software: We have a special application that link 3 MCU with CAN bus. 2 MCUs are on the same PCB( 2" by 2"), the other one is on a separate PCA only 3" away connected by a short cable…