Part Number: ISO1228 Dear Sirs, I'm trying to use the nINT pin as an interrupt, connected to a pin on my microcontroller (MCU), to read the input state only when there's a change. However, the nINT pin is always low. Does this pin need a pull-up resistor…
Part Number: ISO1228 I am designing ISO1228 input stage with the wire break detection function . Sorry, I am not clear about the wire break resistor (RIWB).
I would like to put this resistor in the board. Is it a pull down resistor as R151 or a pull…
Part Number: ISO1228 Other Parts Discussed in Thread: ISO1211 Hello team,
Im currently working on FMEA of a design using the ISO1228 digital input iC. Do you have FMEA data avaiable for this part? Do you perhaps have FMEA information for supporting…
Part Number: ISO1228 Dear Technical Support Team,
I am currently working with the ISO1228 digital isolation device and would like to confirm whether our chosen external resistor values are appropriate for safe and reliable operation.
Our configuration…
Part Number: ISO1228 Other Parts Discussed in Thread: ISO7740 , ISO1640 , ISOM8110 , ISOM8610 , ISO6760-Q1 Tool/software: Hi Team,
I'm designing a card which need isolators to for isolating by Digital IO and one-wire signals
Can you suggest the…
Part Number: ISO1228 Other Parts Discussed in Thread: ISO1212 , Tool/software: HI SIR
Due to the product consistency
may i know if the iso1228 can support the Source//Sink in the same board?
we don't want to Divided into two boards
thanks
Part Number: ISO1212 Other Parts Discussed in Thread: ISO1228 Hi,
I'm using the ISO1228 configured for source inputs and the ISO1212 configured for sink inputs in a 28VD aerospace application.
While reviewing the datasheets, I noticed the recommendation…
Part Number: ISO1228 Dear Sirs, I'm trying to use the nINT pin as an interrupt, connected to a pin on my microcontroller (MCU), to read the input state only when there's a change. However, the nINT pin is always low. Does this pin need a pull-up resistor…