Part Number: ISO5451 I am using gate driver 1ED020I12-F2 Infineon make and IGBT is FP35R12KT4
I want to replace 1ED020I12-F2 with ISO5451 but the concerns are as follows.
Min voltage required to operate ISO5451 is minimum 15 V and typical or nominal voltage…
Part Number: ISO5451 Team e2e,
I am simulating ISO5451 model in TINA TI. Acc to the datasheet, the input hysteresis voltage at IN+ is typically 0.15 * Vcc1 -->
In my test case, Vcc1 = 5V, hence hysteresis V = 0.75V, which means that the switching…
Part Number: ISO5451-Q1 Other Parts Discussed in Thread: UCC21750 , ISO5451 Hi team,
Does ISO5451-Q1 has a time, during the time this IC ingore the RST signal until this time end, like FLTMUTE time shown below in UCC21750?
Thanks and looking forward…
Part Number: ISO5451 Team e2e,
I am looking for the Pspice model (CIR/MOD/LIB/TXT file in particular) to be imported directly in TINA TI using Macros wizard. I found some files here --> https://www.ti.com/product/ISO5451#design-development but none of…
Part Number: ISO5451 Dear Teams,
My customer is asking what is the resistor value on the internal RST pin? The reason they are asking is because they have a reset signal with maximum output current capability 50mA. They are wondering whether it can successfully…
Part Number: ISO5451-Q1
Hi Team,
We received a query from customer asking for the following information about the 9.3.2 Active Output Pull-down in the datasheet. For me to not miss any information from our customer, I will be copying the complete query…
Part Number: ISO5451 hi team
My customer is using ISO5451 in their project and the PWM goes to STO from MCU and then goes to ISO5451. Due to voltage drop over the long distance, sometimes ISO5451 has no signal output. do you have any suggestions to solving…
Part Number: ISO5451 Hi Team
I have a question about a recommended connection for DESAT pin in ISO5451, where I should to connect a zener diode in parallel to the 220pF capacitor and I'd like to know how I could calculate the reverse voltage in Zener that…
Part Number: ISO5451 My application is single pulse for few mS, I think the desat function might not be able to use, could you please let me know the control signal timing for the inside MOSFET connected to DESAT pin?
Thanks,
Hailong Xu