Hi Nandha,
Please find my replies
Regarding ISO3082DWR :
1. The maximum driver current is 60mA and Icc2 consumption is 15mA. So the total comes up to 75mA on right side per device, 2 devices will need 140mA. you can explore our newer parts like ISO1410 with…
Other Parts Discussed in Thread: ISO6720-Q1 , ISO6720 , ISO7710 Hi Team,
Can you please advise with best alternatives to VOL617A-4T?
Thanks in advance
Best Regards
Furkan Sefiloglu
Hi Kygo,
Thanks for reaching out.
ISO7220 is one of our very old isolator families, I recommend using devices from newer isolator families. ISO6720 and ISO6720-Q1 are the most suitable devices to be used, please go ahead and suggest these two to customer…
Part Number: ISO7820 Other Parts Discussed in Thread: ISO7720 , ISO6720 50kHz, 5V PWM signal input and 3.3V, 50kHz signal output, VCCi is 5v and VCCo is 3.3V, can this part support that? or can you suggest some part support that.
Thx
Part Number: ISO7320FC Other Parts Discussed in Thread: ISO7720 , ISO6720 Hello,
We would like to know if it's possible to power the ISO7320 with differents power supplies on input side and output side, vcci = 5V and vcco = 3.3V and reciproquely. This…
Other Parts Discussed in Thread: ISO6721 , ISO6720 Hello,
Can you tell me if TI has an equivalent to the HCNW2211 Broadcom / Avago p/n but with higher storage temp (+125 deg C)? Thanks!
Best,
Adam
Part Number: ISO1541 Other Parts Discussed in Thread: ISO6741 , ISO1641 , ISO6721 , ISO6720 Hi
Could you help check the ISO1541 schematic as below and any need to adjust ,Thanks
Quickly find solutions to common questions about digital isolator devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
FAQ: Isolation >> Digital Isol…