Part Number: ISO6731-Q1 Other Parts Discussed in Thread: TMS320F280037C I am using this type of isolator having signal DSP_CAN_RX and DSP_CAN_TX , which is connected to TMS320F280037C controller. I want to know the
1. Max DSP_CAN_TX transport delay…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: ISO6731-Q1 , , ISO6731 , ISO6721 , ISO6720 , ISO6521 , ISO6520 Tool/software: Hi team,
My customer wants to find a suitable digital isolator and co-work with TCAN1044ADRQ1. Can you recommend more…
Part Number: ISO6731 Other Parts Discussed in Thread: ISO7731 , , , ISO7731-Q1 , ISO7831 , ISO7331-Q1 , ISO7741 , ISO7742 Hi Team,
Our customer is in dire need of ISO6731 or an alternative for this device. I looked at our products list and the drop…
Part Number: TLIN2021A-Q1 Other Parts Discussed in Thread: ISO6731 , ISO6741 , TMUX7219-Q1 Hi,
See I have one master and two slaves, some time one slave switch to master that time I need to isolate main master. Is there any possible way to isolate main…
Part Number: ISO6762 Hello,
we were wondering, why the ISO6762 is neither listed in the UL File No. FPPT8.E181974, nor in the UL-CA-L181974-24-32205102-8, even though it is mentioned under "PRODUCTs COVERED" in "USR/CNR - Single Protection, Non-Optical…
Hi Hyejeong,
These devices have already completed certification. The datasheet update is in progress, but I do not have a firm date to provide. Please see attached certifications for these devices.
E181974-Vol4-Sec6-20260312_CoC.pdf E181974-Vol4-Sec1…
Hi Tom,
Please see attached the updated UL certificate. It lists ISOM8111 (DFS package) at 5000 Vrms.
I'll be posting this certificate online within the next month.
Thanks, Saleem Marwat
UL Certificate of Compliance File E181974 Vol 4 Sec 6.p…
Conor,
I will work to get answers on the above, but our systems and product teams are still largely out for the holiday, so it may take some time to run this down.
As far as I am aware. I do not believe we have a published certificate specifically…