Part Number: ISO7041 Tool/software: I'm working on an NRTL certification for a device using the ISO7041 and going through the usual hassle of the harmonized standards-but-not-really-because-we-want-your-money issue for hazlocs.
Any chance you have…
Part Number: ISO7041 I would like to use the ISO7041 or ISO7041-Q1 to send gate drive signals to high-side device in a half-bridge in an automotive application. However, the data sheet states a working voltage of only 400Vrms and I may have a working voltage…
Part Number: ISO7041-Q1 In datasheet (SLLSFN3 / June 2023) there are Table 5-1 :
ISO7041-Q1 Automotive, Ultra-Low Power Four-Channel Digital Isolator datasheet
"Input, channel A-D. 300-Ω series resistor recommended "
and same for output channels…
Part Number: ISO7041 Hi Team,
There is one channel which will not be used in the design. To have the lowest power consumption, should the IN pin be a no connect, pull-up, or pull-down resistor? The default output is high and from https://e2e.ti.com/support…
Part Number: ISO7041-Q1 Other Parts Discussed in Thread: ISO7041 , ISO6741-Q1 We plan to use the digital Isolator ISO7041-Q1 – and / but we need a supply voltage of 1.8V.
On the TI-webpage we can search/filter for digital isolators with 1.8V and…
Hi Lars,
Thank you for your patience and sorry for the long wait while we contacted the design team.
As you observed, the ISO7041-Q1 does not have refresh EN1 and EN2 pins for pin 7 and pin 10 respectively. The refresh feature is always enabled for the…
Part Number: ISO7041-Q1 Other Parts Discussed in Thread: ISO1640 , ISO7041 I need low power ibidrectional I2C cominication , ISO1640 is usefull for this aim,but power consumption is high, so I want to design I2
C isoleted cominication with digital isolator…
Part Number: ISO7041
Dear Sir or Madam
We are using your digital isolator ISO7041 as a part of the Explosion-proof equipment that we manufacture (it is IECEx certified).
Currently, I work for acquiring Korean certification (KCs certification) for it…
Part Number: ISO7041-Q1 Hi Expert,
Customer want to use ISO7041QDBQRQ1 for LIN communication isolation. See the block diagram as below.
Do we must need to add a 300 Ω series resistor in our LIN isolation application? What is the purpose of 300ohm…