Part Number: ISO7041-Q1 Other Parts Discussed in Thread: ISO7041 , Team,
ISO7041 and ISO7041F are ATEX certified (per certificate CSANe 20ATEX2003U).
How about ISO7041-Q1, is it also ATEX certified, or not?
Thanks for your help.
Part Number: ISO7041 Hi Team,
There is one channel which will not be used in the design. To have the lowest power consumption, should the IN pin be a no connect, pull-up, or pull-down resistor? The default output is high and from https://e2e.ti.com…
Part Number: ISO7041
Dear Sir or Madam
We are using your digital isolator ISO7041 as a part of the Explosion-proof equipment that we manufacture (it is IECEx certified).
Currently, I work for acquiring Korean certification (KCs certification) for…
Part Number: ISO7041-Q1 Other Parts Discussed in Thread: ISO7041 , ISO6741-Q1 We plan to use the digital Isolator ISO7041-Q1 – and / but we need a supply voltage of 1.8V.
On the TI-webpage we can search/filter for digital isolators with 1.8V and the…
Part Number: ISO7041-Q1 In datasheet (SLLSFN3 / June 2023) there are Table 5-1 :
ISO7041-Q1 Automotive, Ultra-Low Power Four-Channel Digital Isolator datasheet
"Input, channel A-D. 300-Ω series resistor recommended "
and same for output channels…
Part Number: ISO7041 Other Parts Discussed in Thread: SN6501 , SN6505B , ISOW7741 Hello
I need your help
I have conneted a ISO7041 to my board
I have one Power supply connected to the VCC1 ( Pin number 1) I have connected all other GND as well as…
Part Number: ISO7041-Q1 In the datasheet of the ISO7041-Q1 in the chapter “8.4 Functional Modes” there is the input “Refresh enable ENx” shown but the device has no such pin.
? Question 1a: Does the outputs “OUTPUTx” also have a undetermined state depending…
Part Number: ISO7041-Q1 Hi Expert,
Customer want to use ISO7041QDBQRQ1 for LIN communication isolation. See the block diagram as below.
Do we must need to add a 300 Ω series resistor in our LIN isolation application? What is the purpose of 300ohm…
Part Number: ISO7041 Dear TI Guru,
When VCC1 (Pin1) and VCC2 (Pin16) are un connected in ISO7041, still the currents flow through GND1 (Pin8 ) and GND2(Pin9) though the IO lines at both sides are floating.
The currents are of the order of 2mA & 4mA…