Part Number: ISOW7840 Other Parts Discussed in Thread: SN6505B , SN6501 Using ISOW7840 with LMV7235M7 comparators on isolated side. The comparators sometimes draw extra current at power-up (latch-up?) causing ISOW7840 to go into current limit. If sufficient…
Part Number: ISOW7840 Other Parts Discussed in Thread: UCC21520 , SN6501 Tool/software: WEBENCH® Design Tools I need an information about ISOW7840 isolation IC. I have a pulse gate signal that drive a nmos switch. I must isolate this pulse with ISOW7840…
Hi Vignesh,
ISOW7840 has two sections of circuit, there is side1 referenced to GND1 and there is side2 referenced to GND2. The two circuits are isolated and can have a potential difference of upto 1kVrms. This means that whether the voltage difference…
Part Number: ISOW7840 Hello expert,
My customer would like to know if OUTx will be pulled high to VISO level when OUTx is floating. From block diagram, this is not related voltage level but I would like to double check. Thanks a lot!!
Best regards,
Ann…
Part Number: ISOW7840
We're using the ISOW7840DWER to isolate a digital signal prior to it reaching the transmitter. While it appears that we've set up the chip correctly we see that one or two bits of the 32 bit message drop low regardless of the decoupling…
Other Parts Discussed in Thread: ISOW7840 On another support thread a TI engineer suggested potentially stacking multiple digital isolators to achieve higher isolation voltages:
e2e.ti.com/.../851658
As the voltage experienced by each one off the isolators…
Part Number: ISO3086T Other Parts Discussed in Thread: AM26LV32E , ISOW7840 , ISOW7740 , AM26LV31E , AM26C31 , AM26C32 , SN65C1167E Hi team,
As show in blew picture, the four single-end SPI signals need to be transferred to differential signals after isolated…
Part Number: ISOW7840 Hi Koteshwar,
I am referring the SLLA368B application note for ISOW7840 for Low Emission design. On Page 7 of document it mentions 0.66 mm creepage distance between two Isolated GND ( GND1 and GND2) .
1) Can you tell me this 0.66 …
Part Number: ISOW7840 Hi
ISOW7840 can not be tied together according to following thread.
https://e2e.ti.com/support/isolation/f/1013/t/806337?ISOW7840-Can-parallel-devices-for-higher-power-supply-output-current-
What is happen if the isolated supply…