Hi,
Can you confirm your chip is ES2.0 silicon and not ES1.0 silicon? You will have to read from the part number on top of the chip. Please refer to https://www.ti.com/lit/ds/symlink/iwr1642.pdf and see what "PG Revision" your part is.
Regards…
Part Number: IWR1642 Other Parts Discussed in Thread: IWR6843 Hello Champ,
As per https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/762440/iwr1642-does-people-counting-demo-has-a-real-time-tracking-lag , it seems that people counting on xwr1642…
Part Number: IWR1642 Dear Sirs:
Per the TRM for 16xx
p293, DSPCLK is from PLLCLK_600 which is divided from PLLCLK_1200. But I didn't see any multiplier or divider registers inside the TRM to describe.
I want to know is there any PLL divider register…
Part Number: IWR1642 Hi Team,
Recently, when I used IWR1642, I found that the initialization of CAN would fail under the following conditions. (The program was stuck in CANFD_init(), and the SDK used was mmwave_sdk_03_05_00_04.)
Condition 1. I used…
Part Number: IWR1642 Hello,everyone.I think i need you help.Thanks!
When I tracked the vehicle with iwr1642, I found that one vehicle became two vehicles side by side during the movement, and their distance and speed to the radar installation location…
Part Number: IWR1642 Hi Team,
Good day! Our customer is asking for IWR1642 single-chip 76-GHz to 81-GHz mmWave sensor integrating DSP and MCU evaluation module. It works on FMCW input freq. setup I was wondering if we can change it to SFCW. is it possible…
Part Number: IWR1642 Other Parts Discussed in Thread: AWR2243 Following my previous question regarding the standard deviation of RF phase differences between two IWR1642 devices, following a common SYNC_IN trigger: 1) Is the RF phase (and frequency) difference…
Part Number: IWR1642 Hello,
I bought the iwr1642boost and I have been testing it with the Labs. Now that I know how it works, I want to do a PCB design with only the sensor iwr1642 and connect it to another microcontroller. What do I have to do? I can…
Part Number: IWR1642 Dear Sirs:
we found there is a low power mode lab in industrial toolbox fundamental. However the libsleep and mmwave link provided is in binary format only. In mmwave_sdk_03_06_00_00-LTS, the library is also only in binary. Can TI…
Hi,
I click the resolved button by mistake.
I've checked the SOP line several times and there's nothing wrong with it. One of my custom boards (Board A) works in functional (SOP4) mode, even when set to Flash (SOP5) mode (1-0-1).
Another custom…