Part Number: IWR6843 Tool/software: Hello TI experts,
I am currently investigating the working principle of FMCW-TDM radar for speed and angle measurement using the TI IWR6843AOP.
I am currently unsure how it is even possible to compare the IQ phase…
Part Number: IWR6843 Tool/software: Hi,
I'd like to make new project that are mss and dss, but i'm not sure how to set that. For example, Compiler version and so on. Do you have any document about project settings to develop IWR6843?
Part Number: IWR6843 Tool/software: Hi,
In order to customize and run the IWR6843, I copied the demo project to another folder and tried to import it with CCS.
However, the message attached is displayed and the project cannot be imported.
Why can't I…
Part Number: IWR6843 Other Parts Discussed in Thread: IWRL6432 Tool/software: Why can IWR6843 only transmit 4GHz from 60 to 64GHz? While other devices can transmit 7GHz such as IWRL6432.
Best Regards, Thanks.
Part Number: IWR6843ISK
Tool/software:
Hello, I am currently applying additional algorithms to the existing Vital Signs demo provided by TI in CCS (Code Composer Studio).
It seems that the main variables used in the core interframe processing function…
Part Number: IWR6843 Other Parts Discussed in Thread: UNIFLASH , , Tool/software: Hi,
Is there size limitation on image for uniflash to burn it on QSPI for IWR6843?
Customer failed to burn 1MB image to flash by uniflash.
Thanks,
Chris
Part Number: IWR6843 Tool/software: Hello TI,
I'm using high accuracy level sensing example.
I want to transmit only target result over DATA_Port without using visualizer : High Accuracy Visualizer (ti.com)
So I want to handle target result information…
Part Number: IWR6843 Hi,
I am using IWR6843 radar module. I want to set the FOV of radar which is not symmetric. Not like -17 to 17 degrees or -60 to 60 degrees. I want to set it to -17 to 50 degrees or -60 to 90 degrees.
Using such asymmetric combination…
Hello Yejean
Can you help me of understanding of binary data of 3D_People_Count ( 3D People Tracking User Guide (ti.com) ) In this can you guide how it counts size of each TLV means in Target list it showing size is 672 bytes. what information contain in…
Part Number: IWR6843
Tool/software:
Hi,
Can user call UART_write and UART_read for one UART port in different task when DMA is enabled?
It seems this will cause issue. Why?
Thanks,
Chris