Part Number: PROCESSOR-SDK-AM62A Other Parts Discussed in Thread: SK-AM62A-LP Tool/software: Hello Team,
MCAL Package: MCAL_SitaraMPU_09.02.00.05
Board: SK-AM62A-LP Starter Kit
We are working to perform Flash operations on AM62Ax device.
As per MCAL_SitaraMPU_release_notes…
Part Number: PROCESSOR-SDK-OMAPL138 Tool/software: Hi,
I used dd command for cloning my custom created SD card. After cloning I powered custom board with SD card. But booting freeze before "Starting Kernel" Message. Console is waiting for an input…
Part Number: PROCESSOR-SDK-AM64X Tool/software: Hi team,
I was actually using the IPC rpmsg between the A53 and the remote core. According to the patch released recently to use multiple endpoints i have tried out with additional end points 15 and 16…
Part Number: PROCESSOR-SDK-AM64X
Tool/software:
Hi community.
I'm Chan Kim and I want to integrate linux-kernel from TI's git repository(git.ti.com/.../refs).
I downloaded the "ti-linux-kernel-6.9.1" from the repository and replace it to "ti…
Part Number: PROCESSOR-SDK-AM62X Tool/software: Hello, I am trying to test read/write GPIO Port Expanders via i2c on the EVK AM62X-LP but I am not sure if the command is right, considering the address 0x22 0x23.
Could you please explain, for instance…
Part Number: PROCESSOR-SDK-J721S2 Tool/software: Hello TI experts,
When I execute /opt/vx_app_arm_remote_log.out, a lot of VX_ZONE_INFO messages of ownTargetNode and ownTargetKernel come in flood.
Those messages don't go away even if I add tivx_clr_debug_zone…
Hi Rejin,
I was saying that this is the expected and intended response. You shouldn't be able to access the device when it is busy.
You will have to disable the driver that is controlling the device.
The only reason i2cget works is because you are…
Part Number: TDA4VM Tool/software: Hello
Would you please tell me where I could download DCC Tuning Tool and related documentation?
I submitted a request through this link: https ://www .ti .com /secureresources /ADAS -SW -IMAGING , but it has been pending…
Part Number: PROCESSOR-SDK-AM62A Tool/software: Please combine two sources (camera frames and graphic overlays) into one image using hardware pipelines.
1. How can I get started with QNX? I am requesting a QNX build.
Can someone please take this up and…