Part Number: LDC1051 Other Parts Discussed in Thread: LDC1614 Hello all,
I am interested in building a data aquisition circuit for a sensor I have been developing in which a signal is generated from a change of inductance (~1-5 nH) based off of a physical…
Part Number: LDC1051 Other Parts Discussed in Thread: LDC1101 , LDC0851 Is the maximum proximity measurement for the LDC1051 limited to 128 (7 bit)? I see that the resolution is 8 bit in the datasheet however I can't read a value greater than 128 in my…
Other Parts Discussed in Thread: LDC1051 , LDC1612 , LDC1614 , LDC1312 , LDC1314 , LDC1101 Hi
I would like to know LDC1051 design for supporting customer.
In datasheet of LDC1051, 8.2.1.2.3 shows how to choose filter capacitor, the waveform difference…
Hello Takahashi-san,
The formula listed above is an approximation to give a ballpark estimate. The actual switching data is based on the inductance ratio between the LSENSE and LREF coils which can be simulated for a given target distance or simply prototyped…
Hi Kris,
my suspicion is that any of the abs max ratings in the electrical characteristics are violated while hot-plugging the device. Please use a scope to find out which of the pins violate the abs max ratings.
Pins 14 and 15 of the LDC1051 are physically…
Other Parts Discussed in Thread: LDC1051 , LDC1312 , LDC1612 , LDC1614 , LDC1314 , LDC1101 Dear Sirs
Is LDC1051 NRND?
Do you recommend other Inductance to Digital Converter solution?
BRS
Nat
Other Parts Discussed in Thread: LDC1051 Hi,
Just received my LDC1051 EVM, I have watched the intro vides and gone through the FAQs in the Forum. I have two questions before I can plunge into the world of TI devices:
1. What is the difference between…
Other Parts Discussed in Thread: LDC1051LDC1051 is evaluated.
Although it operates normally at 25℃, it becomes oscillator overloaded and stops at 45℃.
(Register table 13)
If a mistake occurs about a setup of LDC1051, please let me know.
・A setting…
Other Parts Discussed in Thread: LDC1051 Please let me know two points below about LDC1051.
-------------------------------------------------------------------------
・OSC (Address:0x20)
What kind of cause does OSC set to "1"?
(After operating…
Other Parts Discussed in Thread: LDC1051 Please let me know two points below about output register and Rp_max of LDC1000 and LDC1051.
・Is a LDC output register a maximum of 8bits(255)?
Although outputted only to 7bits(128), what is reasonable ?…