Part Number: LDC1101 Hello,
Is it possible to form the resonant LC section with capacitive probe and a fixed inductor or some coax . The resonant frequency would be modulated with the change in capacitance rather than inductance, the LDC1101 wouldn't know…
Part Number: LDC1101 I am not getting any LP or Rp Data. Am i missing something? can anyone help me? below is my config param.
int8_t ldc1101_init() { uint8_t chip_id;
// chip_id = ldc1101_readByte( _LDC1101_REG_CHIP_ID ); // if( chip_id != 0xD4 ) // { …
Part Number: LDC1101 Hello,
We are using the LDC1101 to design a padlock presence sensor.
On a metal bar, there is a hole of 15mm, where the padlock is inserted. The padlock lock diameter can vary between 1 & 14mm. we are looking to put thin coil around…
Part Number: LDC1101 Other Parts Discussed in Thread: LDC1001 , , TDC7200 Hello there,
I would like to compare here LDC1101 and LDC1001 in LDC DRDY Timing measurement. All based on SNOA941A App Report and LDCs manuals SNOSD01D and SNVSBF7 . I want to use LDC1x01…
Part Number: LDC1101 Hello,
I have an application where the LDC1101 is embedded in a very small device alongside the measurement coil. The inductance measurement is intended to reflect the position of a moving piece of metal. There is a small microcontroller…
Part Number: LDC1101 Other Parts Discussed in Thread: LDC1041 , LDC1051 Hi TI, I am using ldc1101 for metal distance measurement, The inductance is a ferrite wire wound inductor with a diameter of 26mm. The maximum sensing distance is 15mm. L: 70uH; C…
Part Number: LDC1101 Other Parts Discussed in Thread: LDC1312 , Hello there,
I would like to ask how the measurement method differ between LDC1101 and LDC1312?
Lets say we have both devices (LDC1101 in LHR mode and LDC1312 in single channel mode) set to…
Part Number: LDC1101 Hello I am using the LDC1101. According to the datasheet the device should start giving conversion results when the device is put in active mode. I am interested in Rp results and the registers 0x20, 0x21 & 0x22 don't change even though…
Part Number: LDC1101 Other Parts Discussed in Thread: LDC1041 , LDC1001 Hello,
I am currently working with the LDC1101 and am getting nice data out of it. I would like to speed things up and switch to DMA + interrupt driven polling on my ST micro, and…