Hello Justin,
could you give a specific absolute accuracy for the high/medium/low resolution.
For example, I use LDC1612 to measure the distance of an object, what are the corresponding values of these three precisions?
looking forward to your reply.
Part Number: LDC1612 Some questions about LDC1612 register configuration. I want to use a function like this: 1. Only use CH0; 2. Full precision conversion time; 3. The INTB Pin generates a falling edge interrupt when the conversion is complete; My register…
Part Number: LDC1612 There is a question about coil diameter and detection distance.
Can the following two conditions of use achieve similar stability and detection accuracy?
1. Use a 20 mm diameter coil to detect 8mm in diameter;
1. Use a 13.9 mm diameter…
Part Number: LDC1612 Some questions about LDC1612 register configuration. I want to use a function like this: 1. Only use CH0; 2. Full precision conversion time; 3. The INTB Pin generates a falling edge interrupt when the conversion is complete; My register…
Part Number: LDC1612 Hi TI Team,
I am working on a solution with a LDC1612. The system is very sensitive and the target movement is as high as 1.5 mm. With this system i cant find a IDRIVE0 setting to hold the amplitude between 1.2 V and 1.8 V. I tried…
Part Number: LDC1612LDC1612 has operating voltage of 2.7V to 3.6V. For a particular set of LC value and environment, will the measurement result change if the operating voltage changes from 3.7V to 3.6V ? Thanks.
Part Number: LDC1612 Other Parts Discussed in Thread: LDC3114
Dear Community,
I want to use the LDC1612 IBIS model to simulate the output envelope waveforms on both channels with different input clock frequencies.
My questions are:
1) Is this possible…
Part Number: LDC1612 Hi,
In my design I am using LDC1612QDNTTQ1 part, Can you please support on Rectangular coil design calculation ? and also suggest which one, circular or rectangular coil shape is good ? for more range detection. I am using 4 layer PCB…
Other Parts Discussed in Thread: LDC1612 Hai all,
I am currently working on inductive sensors for longer sensing range and I came across LDC1612/1614 as a solution for the same.
But, while going through the datasheet I have a few queries:
1) what is the…