Part Number: LM10504 Hi,
It would be very appreciated if you answer following questions about Buck1 from our customer.
1. How does Buck1 work when Vin <3.5V is met and Vin ≥ Vout + 1V is not met?
Is Bypass-FET Operation prioritized and not switching…
Part Number: LM10504 Hi,
I have question.
The data sheet P18, 7.3.8 Low Dropout Operation states "The device can operate at 100% duty cycle (no switching; regulator switch completely on) for low dropout support."
But, the data sheet P7, 6.6…
Part Number: LM10504 Hello,
We want to control LM10504 output turn on time in some reasons. Is there any options to control ramp up time?
Best regards,
Toshihiro Watanabe
Part Number: LM10504 Other Parts Discussed in Thread: TPS65218D0 , TPS65023B Hello,
LM10504 is now NRND on TI.com. Then my customer has 2 questions.
1. Does TI have EoL plan for this device today?
2. Does TI have alternative recommend part?
For 2, if we…
These are Murata multi-layer power inductors.
The closest inductor available in the lab here at TI is the MLP2520V1R5M (TDK 1.5uH multi-layer inductor rated for 1.4A)
I tested the LM10504 EVM with the default VLF3010ST-2R2M1R1 2.2uH inductor, then swapped…
Part Number: LM10504 Other Parts Discussed in Thread: TPS65023 , LM10506 Hi,
I was wondering, if it is possible to program the LDO to supply another voltage at power up? As it is now, the voltage is 3.0V, but I need 3.3.
Is that possible?
/Bent
Part Number: LM10504
Hi,
I received the following question from my customer.
What should we do anything (i.e. pin termination, register setting...) when the LDO is not used?
I'm recognizing the "LDO sleep mode "register.
Best Regards,
…
Part Number: LM10504
Hi,
Abnormally switching is occurred on customer's board
I attach the switching waveform of the BUCK1 and the condition is following;
Board:Customer's board
Vin:5V
BUCK1:3.3V、200mA
BUCK2:1.8V、200mA
BUCK3:1.2V、700mA
Ta:Colder…