Part Number: LM117QML-SP Tool/software: Hi,
In the absolute maximum ratings section, app note (2) stated that the power dissipation is internally limited, but the specifications are applicable for power dissipations of 2W for the TO-39 and CFP packages…
Part Number: LM117QML-SP Other Parts Discussed in Thread: LM117HVQML-SP , , LM317 Tool/software: Hello, I wanted to know if there is any Spice model for the LM117QML-SP or the LM117HVQML-SP!
Thanks!
Part Number: LM117QML-SP Tool/software: Hi,
Greetings!
Can we connect the NC pins of LM117-SP (16 Pin CFP SOIC) IC to ground plane?
Thanks in advance.
Regards,
Ankit Singh
Part Number: LM117QML-SP Tool/software: Hello.
The Iadj spec in the LM117HRLQMLV (5962R9951705VXA) datasheet is a negative current. Does this mean that the LM117HRLQMLV device sink current? And, The Il (load current) is also a negative current. Why…
Part Number: LM117QML-SP Hi,
The customer needs SELET information.
TID information is written on the data sheet, so you can check it.
However, there is no SEL LET information, so I request the information.
Part Number: LM117QML-SP Hello,
A recent circuit card failure has been traced to P/N 5962R9951707VZA and the failure analysis lab has requested the device schematic to support the investigation into the device failure. We reviewed the simplified schematic…
Part Number: LM117QML-SP Hi,
I am thinking of using the LM117QML-SP linear to pass or limit an unregulated voltage bus, 28V ≤ VBUS ≤ 36V, to be ≤ 32V.
I estimate the maximum load on the output of the LM117QMP-SP to be around 9.15W.
I would like…
Part Number: LM117QML-SP Hi Experts, I am checking the difference of the 2 devices below: 5962R9951707VZA - Texas instruments 5962R9951705VZA - National semiconductor It seems that they are the same device. Can you also confirm that they are the same…
Part Number: LM117QML-SP
Our customer requires an instantaneous output of about 2.1A for about 1e-4 seconds. Will the LDO be able to sustain such load without suffering any long term damage?