Part Number: LM118-N Tool/software: Hi,
I have a query regarding a part number LM118-N. This is not a orderable part number but this part number is mentioned in datasheet. Also can you confirm us what is that "-N" denotes? Because I couldn't find…
Part Number: LM118-N Other Parts Discussed in Thread: LM119QML , LM119 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
I need to build a comparator with the op-amp LM118H. The signal bandwidth is 15 MHz. But the problem is…
Part Number: OPA928 Other Parts Discussed in Thread: LM118-N , OPA191 , OPA2191 Tool/software: Hi,
I am supporting my customer with the design of a constant current source which outputs 500uA to a 20k ohm load. It receives a 16V power supply to the…
Yuto-san,
LM318 model
http://www.ti.com/lit/zip/sloj042
LM118-N model
http://www.ti.com/lit/zip/snom265
LM318-N model
http://www.ti.com/lit/zip/snom245
Teja C,
That is a design from 1973 using an all but obsolete op amp, LM118-N; so there are better ways to perform this function now.
What is your LM324 supply voltage? +/-15V is recommended for this design.
I'll start with A1, for positive input…
Other Parts Discussed in Thread: LM318 I am trying to build a simple subtraction amp like figure 45 of the LM318 data sheet. attached (I think). I need to subtract 2 sine wave signals both of which are 6.78 MHz. I have bypassing on the power supply, and…
Hello Jack,
Oh...that's an oldie..
Essentially it is a 30MHz un-compensated amplifier that allows you to add your own compensation cap to set the BW. That's the way it was done before internally compensated amps became popular (aka: the "new fagled…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…