Part Number: LM135 Tool/software:
Our customer has us cut off the ADJ leg of the LM135 and just wire the +V and -V terminals in parallel to a capacitor, which is in turn wired to leads to a connector.
The LM135/capacitor is then inserted into a…
Part Number: LM135 Tool/software: I am trying to use the LM135H in a vacuum environment, is there a document that lists the mass/surface area breakdown of everything in the package?
Thanks,
Matt Bailey
Part Number: LM135 Is there a radiation hardness data for LM135 series temperature sensors ?
I am referring to gamma radiation hardness total integrated dose (TID) in rads or Gy. No data was listed in closed link below:
https://e2e.ti.com/support…
Part Number: LM135 Other Parts Discussed in Thread: LM95172-Q1 Hello,
I'm using a temperature sensor LM135AH for a wide-temperature measurements ranging from 25°C - 175°C. I'm attaching the schematic below, In previous designs, I used the 5V rail…
Part Number: LM135 Hello team - could you please help me understand the differences between the LM135H and the obsolete LM135H-MIL? If we were to move a design from the LM135H-MIIL to the LM135H would any changes/updates be required?
Thank you!
Part Number: LM135 I need to measure the temperature of a Temp/Vac chamber. I want to use the LM135/135A
It sits inside the chambers and drives about 7' of wire to a board with a A/D converter. My power supply is either +3.3V or +5V.
The problem is…
Hello Aaron,
PIND testing is not performed on commercial grade products.
LM134H will be the part with SnPb lead finish.
LM134H/NOPB will have not Pb (lead).
Part Number: LM135A Hi Team,
We received inquiry from customer asking the difference of between typical and maximum accuracy specification.
Also, what sigma (1,2 or 3?) used for typical and maximum accuracy?
Thank you and looking for your kind response…
Part Number: LM135 The reads on this temp probe is going from room temp which is about 22.8C to 75C. Once we hit 75C the temperature starts to read in a descending reads. All the way in the -200+C. On my conversions I have it as (Value*100)-273. This…
Part Number: LM135 Other Parts Discussed in Thread: LMT87 ,
Hi Team,
Say in one case, ADC Vs = 3.3V, internal Vref 2.5V is fixed, cannot be changed.
LM135 is used for ThermoCouple - CJC purpose. Then fits the output voltage into ADC for calculation…