Part Number: LM1881 As per previous discussions on the forum, there's no minimum supply voltage listed so we can only assume it's 5.000V. The application circuits use a 5V supply - have we to assume there's no droop what-so-ever on this? That seems like…
Part Number: LM1881 Hi team,
picture 1
picture 2
Figure 1 shows the output waveform of el1881 I used before,
Figure 2 shows the output waveform of lm1881mx,
The output waveform of lm1881mx has delay. My circuit is designed according…
Part Number: LM1881 Hello,
(Question)
Is LM1881 supported Macrovision signal?
Is the output signal corrupt with Macrovision input signal?
Regards,
Tao_2199
Part Number: LM1881 I need emailed to me a current CMRT REV 5.12 for the parts listed below please.
LM384N/NOPB
LM1458MX/NOPB
LM324DR
LM1881M/NOPB
NE5532ADR
LM13700MX/NOPB
TLV2362IDR
TPS70751PWP
TL3474IDR
TL3472IDR
LM224D
LMM3478MM…
Part Number: LM1881 Hi,
From the datasheet it seems that the Vcc voltage at 8th pin of LM1881 IC ranges from 5 to 12V.
We can understand 12V is the maximum acceptable voltage at this pin.
What is the minimum acceptable voltage at this pin? Is…
Part Number: LM1881 Other Parts Discussed in Thread: LMH1980 Hi team
My customers want to apply the LM1881 as an ISL59885 replacement.
What should be important when reviewing?
Is there any problem to replace it immediately?
Thank you
Part Number: LMH1981 Other Parts Discussed in Thread: LM1881 Hi team,
We are looking for video sync separator like LMH1981.
But only VSOUT is needed. Is there such device?
Best, Zeming
Part Number: LMH1981 Other Parts Discussed in Thread: LM1881 Hi,
We are currently working on a new project which involved and external sync device such as UltraSync One which has a SYNC output that outputs genlock or work clock.
Can we use this…
Part Number: TVP5160 Other Parts Discussed in Thread: LMH1980 , LM1881
Hello
I want to have RGB (with Csync, sync on composite, and sync on green) + YPbPr + S-video + Composite video as inputs then have digital output suitable with ADV7341 (YCbCR…