Part Number: LM1971 Hello E2E Experts,
Good day.
We want to simulate the LM1971 schematic in the P-Spice tool for TI. we want to get the simulation resources to proceed further. Kindly please help us out on the same.
Regards,
CSC
Part Number: LM1971 Hello TI,
I seem to be having the same issue as was reported in the thread below:
LM1971: the max attenuation of lm1971 is about 20db,but attenuation of the datasheet is 62db? - Audio forum - Audio - TI E2E support forums
I have LM1971…
Part Number: LM1971 Recently I created a two channel audio attenuator using two LM1971 s. Everything works fine except mute function. when muted , I can hear the audio slightly from the output .
Design files attached.
Any guidance appreciated.
Thanks.
…
Part Number: LM1971 Other Parts Discussed in Thread: TPA3138D2 "When the µPot is powered up, it is placed into the Mute mode " in datasheet,actually the attenuation we tested is about 20db. even if we set the lm1971 to 62db ,the attenuation…
Part Number: LM1971 Hi Experts,
Customer want to use 4 x LM1971 atten for their project.
For circuit design,
Is it possible to use control signals all in common to control 4x LM1971 ?
Or Is it possible to use tow signals (CLK/DATA) in common and separate…
Part Number: LM1971 Other Parts Discussed in Thread: LF412 , LF411 , LF353 Dears,
My question is, the OPA behind the LM1971 output pin is necessary or not?
As the schematics, I think the OPA just is a buffer which without any gain adjust function.
Therefore…
Other Parts Discussed in Thread: LM1971 Hi Team,
The customer is using LM1971. LM1971 can be attenuation step size from 0dB to -62dB. But when the customer sets LM1971 to be attenuation 0dB,
the output signal is more attenuation than the input signal. Look…
Other Parts Discussed in Thread: LM1971 , LF353 We have a tone generator sysetm, in which I have added LM1971 to control the volume level according to the requirement from a microcontroller. Volume Up and Down are working fine, but during the process, an…
Part Number: TPA3111D1 Other Parts Discussed in Thread: , LM1971 Hello team,
I have received a question from my customer about the popping sound during test of TPA3111D1.
■ Question
When the SD (Shutdown) terminal is set to H (outputs enabled), the speaker…