Part Number: LM25116 Tool/software: Dear Sir/Madam
We have bought an adjustable buck converter device that includes the LM25116 IC. Its RFB2 resistor is a potentiometer and adjusting this potentiometer adjusts the output voltage. Would it be possible…
Hi,
As I have not heard back from you for some time now, I will close this thread. Should you have any new information, please feel free to open the thread and I would be happy to assist you.
Thank you,
Joshua Austria
Part Number: LM25116 Other Parts Discussed in Thread: LM5116 Tool/software: Greetings, previously I've been trying to make a buck converter using LM25116 in this post , using this configuration based on LM5116_Quickstart datasheet:
With this parameters…
Part Number: LM25116 Tool/software: Hello there
Sorry if i write something wrong, english is not my native language.
I am having troubles designing a buck boost with the LM25116, my requirements are:
Vin: 7-42v
Vout:14v
max Iout: 20A
I am planning in…
Part Number: LM25116 Tool/software: Hi team. In the process of optimizing our board design, we have designed a new version for the LM25116 converter board. Can anyone please take some time and review the board and let me know if this can be made any…
Part Number: LM25116 Hi TI expert,
Now I want to use LM25116 to generate a negative voltage.
Total spec is that:
Vin: 12.6V
Vout: -13V
Iout: 3.5A~4A
As for inductor, I want to use SER1360-103KLB(Coilcraft), which is 10uH, Rated current 7A.
As for MOSFET…
Part Number: LM25116 Tool/software: ①In 8.2.2.6 of the datasheet, it says that the input ripple current is IRMS > IOUT / 2, but is it okay to estimate it at a value close to IOUT / 2?
Conditions: Vin 24V Vout 17V~10V Iout 11A, 4A (2 circuit design)
…
Part Number: LM25119 Tool/software: Dear TI,
I am not sure is this is allowed to use NMOS RDSon as the shunt resistor?
If this is possible what filtering RC should be used?
Bests,
Brian
I am closing this thread since I have not heard from you for sometime. If you are still trying to resolve the issue, please feel free to open a new thread. Thanks - EL
I am closing this thread since I have not heard from you for sometime. If you are still trying to resolve the issue, please feel free to open a new thread. Thanks - EL