Part Number: LM25118EVAL Hello,
We are using and have referenced the LM25118EVL board in our design, but we are having some trouble with the reflow soldering of the power inductor.
I know this is not a TI component, but it is the same part as that used…
Part Number: LM25118EVAL Other Parts Discussed in Thread: LM25118 , LM10011 Tool/software: WEBENCH® Design Tools I have a fixed 12v power supply Vin .
Require #1: Can LM25118 produce 12v VOUT?
Require# 2: I like to have Vout programmable in range of 11v…
Part Number: LM25118EVAL Hi Team, LM25118EVAL consists of 4 layers and 3.45 X 2.65 inches of board size. My customer considers to design similar board (input: 5-42V, output: 12V / 3A, fsw=300kHz) with 2 layers at same board size. Is there any thermal issue…
Part Number: LM25118 Hi all:
I have a demo of LM25118,LM25118EVAL。
Demo data shows that the input voltage is 5~42V, and the output current is limited to 0~3A.
Now, I need to change the input to 3V and the output current to 6A.What should I do?
Other Parts Discussed in Thread: LM25118 , LM25118EVAL Hello,
We design the power supply board using LM25118.
Required specifications : Vin=8-28V,Vout=12V/Iout=Max.5A
When Cramp is 1nF with our custom board,MOSFET Switching waveforms are disturbed.(Please…
Thanks for posting your schematic. Do you have waveforms that demonstrate your issue? You can order the LM25118 EVM here:
www.ti.com/.../lm25118eval
The EVM is rated for 12 V out at 3 A.