Part Number: LM25119 Tool/software: Hi TI ,
I would like to Know about LM25119 EN2 PIN,
According to SPEC ,
It Seems to pull up 50k ohm Internally ,
When I used an oscilloscope to measure, I obtained 4.5V.
May I know more information about how 4.5V comes…
Part Number: LM25119 Tool/software: Hello,
I would like to ask you a question about the LM25119's VCC capacitor capacitance. Is there an upper limit to the VCC capacitor capacitance? In the circuit I created, when the load is suddenly increased, VCC…
Part Number: LM25119
Tool/software:
Dear TI,
I would like an offline assist about LM25119 efficiency and thermal 3.3V @ 36A interleave buck design.
Contact Email: briansune@gmail.com
Bests,
Brian
Understood, so TI would propose how much of margin in regarde to UVLO must be lower than 15V.
So 1,87-1.25 is proposing over 0.5V noise spectrum?
This is a huge noise and could this even possible when the VIN pin is already coupled by a 100nF X7R capacitor…
Part Number: LM25119 Tool/software: Dear TI,
I am not sure is this is allowed to use NMOS RDSon as the shunt resistor?
If this is possible what filtering RC should be used?
Bests,
Brian
Part Number: LM25119 Dear TI,
I would like an offline PCB design review and discuss efficiency measurement result.
Please use contact EMAIL:briansune@gmail.com
BR,
Brian
Part Number: LM25119 Other Parts Discussed in Thread: PMP10979 , Hi,
I'm searching for a very high efficiency DC-DC buck converter for a new design, with the following parameters:
Vin = 12V or 24V
Vout = 2.4V,nom
I,out,nom=25A
I,out,max=40A
Searching…
Part Number: LM25119 Hi Ti ,
I have used LM25119 to design 3.3V and 5V power supplies.
Can you assist in checking the schematic and layout placement?
PSB529_Ti.pdf PSB529-LAYOUT.zip
Best Regards,
Joshua
Axiomtek Co., Ltd.
Part Number: LM25119 Other Parts Discussed in Thread: LM5119 , Hi
Is there any difference between TI LM25119PSQ-NOPB and LM5119PSQ-NOPB / LM5119QPSQ-NOPB? Can LM5119PSQ-NOPB / LM5119QPSQ-NOPB directly replace LM25119PSQ-NOPB without changing the peripheral…
Part Number: LM25119 Other Parts Discussed in Thread: LM5119 , Team,
I am looking at possibly using LM25119 as a replacement for LM5119. Looked through the datasheet for any major differences, but they look to be about the same.
But wanted a quick sanity…