Part Number: LM2611 Hello, I recently built a CCA that uses an LM2611AMF CUK regulator. Applied power is 12VDC and Vout set for -3.3V (RFB1 is 16.9k and RFB2 is 10k). My problem is when power is applied to the input of device, it acts as a short circuit…
Part Number: LM2611 Hi Team,
Our customer noticed a missing diagram in Figure 15 in the datasheet of LM2611. According to our customer,
I am trying to determine the component values required for my application, using the LM2611 datasheet, however there…
Part Number: LM2611 Other Parts Discussed in Thread: ALLIGATOR We have the following LM2611 circuit below that is powering a circuit that has a current consumption between 20mA and 80mA (verified by removing the LM2611 and using a bench supply). When we…
Part Number: LM2611 Hi Team,
Our customer would like to confirm if the LM2611 can output 100mA from an input of +9V and output of -30V. It seems like the Webench Power Designer doesn't support this device.
Regards,
Danilo
Part Number: LM2611 Other Parts Discussed in Thread: ALLIGATOR Hi team,
We are using the LM2611BMFX part in our design for converting 12V to -5V.
This power is going to the analog section in our design. We have seen noises in the Analog section & while…
Part Number: LM2611 Other Parts Discussed in Thread: TPS63700 Hi team,
Can you suggest inverting boost converter with the requirements below?
Vin: 5.2V, Vout: -12.4V, Iout: 0.4A
TPS63700 can not draw enough current in this Vin/Vout case. I have submitted…
Part Number: LM2611 Hi,
I am designing a converter around the LM2611 to produce a -12V rail from a 3-5V input. This would give a duty cycle of ~73%, which per the datasheet requires the addition of an extra compensating pole-zero pair in the feedback…
Part Number: LM2611 Hi,
Could you review the schematic for -12V output from 12V?
current is 5mA.
Additionally, what component has to be changed for 50mA current?
Now R16 is 87.5kOhm.
Thanks.
Part Number: LM2611
I want to know how to generate -2.5V with this part. I read the datasheet and I don't see any reference in how to configure the part. 8.2.3.1 Design Requirements This design converts 9 V (VIN) to –5 V (VOUT). Adjust RFB2 to set…