Part Number: TPS65023-Q1 Other Parts Discussed in Thread: TPS65023 , LM26480 Hi,
I was not able to find any PSRR data for the internal LDOs of the TPS65023.
Do you by chance have any data?
Thanks
Regards,
Alberto
Part Number: LM26480SQ-AAEV Other Parts Discussed in Thread: LM26480 , TPS65320-Q1 , TPS65321A-Q1 Hi,
can the IC support spike of 20V?
If no, is there an equivalent IC with input voltage greater that 20V?
Thanks.
Best regards.
Giuseppe
Part Number: LM26480SQ-AAEV Other Parts Discussed in Thread: TPS65321A-Q1 , LM26480 HI,
I need use only one buck and LDO channel of LM26480SQ, and I want to disable unused ones by connecting ENSW2 and ENLDO2 to GND.
in this way will npor go high when the output…
Other Parts Discussed in Thread: TPS659037 , TPS650861 , LP8733-Q1 , TPS65218D0 , TPS65023 , LP87564-Q1 , LM26480 Hi Team,
Does TI have suitable PMIC to replace DA9063(which is use to supply Telechip MCU TCC8031)? Thanks a lot!
The datasheet of DA9063 is attached…
Other Parts Discussed in Thread: CC2642R , TPS65023B , TPS650231 , LM26480 , LP8758-E0 , TPS65218D0 , LP8752-Q1 Tool/software: WEBENCH® Design Tools im looking for low power, 4 output PMIC.
information given below is in the order of;
IC name : Voltage ; Current…
Part Number: LM26480 Other Parts Discussed in Thread: LM26484 , LP873222-Q1 , LP873220-Q1 Hello,
The LM26480 looks to be an almost perfect fit for an application of mine, but the 1.5A on rail 1 is a little tight. Otherwise the 1.5A on rail 2 and the two…
Other Parts Discussed in Thread: LM26480-Q1 Dear all,
if i use LDO2 so that is connect ENLDO2 to 2.5V, VINLDO2 to 1.35V and set the resistors value to get 1.2V on LDO2 output will this work with LM26480-Q1?
in another mater what is the LDO dropout , what…
Hi Alex,
This is a part of a family of successful components; new designs are continued coming in. There is also a -Q1 part for automotive. if you need a dual there is lm3370; dual bucks, dual LDOs- the lm26480 and more. There is a growing demand on these…