Part Number: LM2676 Hi Dear,
Overall length, incl leads is below Datasheet specs. You can refer to details as attached.
DS: 15.12mm/15.36mm
Actual: 14.25mm
also have additional findings:
May 2023 datasheet revision (old rev) stated length measurement…
Part Number: LM2676 Other Parts Discussed in Thread: TLVM13630 , LMR51430 There is no soft start terminal. Does the output voltage reach the set output voltage instantly at startup? Or does it reach the designed voltage with a time constant? I would like…
Part Number: LM2676 Tool/software: Hi,
I wanted to verify which capacitor should I use for the boost cap. The datasheet mentions 2 different recommend values. The "Typical Application" diagram schematic shows a 0.01 uF cap while the "5.1 Pin Functions…
Part Number: LM2676 Other Parts Discussed in Thread: LM2679 Hi,
We use the LM2676-ADJ for the DC/DC buck from 24VDC to 8VDC, and now, we use the LM2679-ADJ with the same design, but the LM2679 has no output voltage, so please refer to below LM2676-ADJ…
Part Number: LM2676
Hi TI team,
Thank you for your support.
I have a question for Overcurrent protection for LM2676T-ADJ/NOPB,
When Environment is
24V as Voltage Output and 1A as current output.
*How much voltage will be drop when…
Part Number: LM2676 The load is too light and the ripple is large. 100mA Ripple 100p-p (mV). Is there any problem in use? And inductor, capacitor error, temperature change, secular variation, When implemented at the worst value of 80uH 122uF, it was 240P…
Part Number: LM2676 Hi,
We test the LM2676SX-ADJ for External Visual Inspection (EVI) and X-ray analysis, 3 pieces were used for SAM, Solderability test and Decapsulation analysis.
Product arrived in reel without appropriate MSL protective packaging…
Part Number: LM2676 Other Parts Discussed in Thread: LM2673 , , LM22676 Dear support,
We need an alternative solution pin to pin compatible for the LM2676SX-ADJ and I found that the LM2673S-ADJ could be similar with same performances (we need 3A without…