Part Number: LM27313-Q1 Other Parts Discussed in Thread: TLV61047-Q1 We are trying to use this part LM27313-Q1 and calculate the power loss and junction temperature based on the application we used. So I have two questions which need support, please help…
Part Number: LM27313-Q1 Other Parts Discussed in Thread: LM27313 , TPS61379-Q1 I was using LM27313 to boost 7.5V to 14.2V following the design guide in the TI WEbench. And I got same testing result as the simulated waveform in the WEbench. So whether…
Part Number: LM27313 Other Parts Discussed in Thread: TLV61047 Please help to review the LM27313XMF/NOPB boost converter section in our schematic.
VOUT: 12 V
IOUT: 0.4 A
Part Number: LM27313-Q1 Other Parts Discussed in Thread: TLV61047-Q1 Dear TI Team,
I would like to request the pin Failure mode analysis data(FMA) for the LM27313-Q1 device for compliance and documentation purposes. Kindly share the latest available…
Part Number: LM27313 Tool/software: Hi All,
I have a question about the LM27313. What is the FET On voltage? Some formulas use the term Vsw, but what is the standard value?
Best Regards, Ishiwata
Part Number: LM27313-Q1 Tool/software: Hello,
Is it possible to use shutdown pin of LM27313-Q1 to enable and disable the IC? I used a enable signal from a controller and connected it to the shutdown pin of the IC. Instead of 1k resistor I used a higher…
Part Number: LMR64010 Other Parts Discussed in Thread: LM27313 , TLV61047 Tool/software: Hi All,
Please tell me the difference between the LMR64010 and LM27313. I would like to know the differences other than the maximum switching current values.
…
Part Number: LM27313 Tool/software: Dears,
Occasional no output, In severe cases, the IC may be damaged, for GND impedance, pin1 and pin5 are open circuits. Can you please check if there are any issues with the schematic.
Part Number: LM27313 Other Parts Discussed in Thread: TLV61047 Tool/software: Bug in the 5V → 16V PWM Booster Controller
Context During thermal chamber tests, it was observed that when ambient temperature reaches 65 °C , the analog I/O system stops…
Part Number: LM27313 Other Parts Discussed in Thread: LM2731 Tool/software: Hello!
Several suppliers offer to buy microcircuits with this marking. The markings have crooked symbols. Is this the original marking? Thank you! Best regards, Jack Barret