Part Number: LM27313-Q1
Tool/software:
Dear [TI Support / Team],
I’ve been testing the LM27313-Q1 on a breadboard to validate whether the design meets the intended specifications. However, I’ve noticed that the output consistently exhibits a high…
Part Number: LM27313-Q1
Hi Team,
The LM27313XQMF is used to regulate 12V from Vin range from 5.6 to 6V.
TINA simulation shows dip in the output voltages regulation whereas in Webench there is no such Voltage dip for the load of 250mA.
Here are…
Part Number: LM27313 Hello Team,
What is the ratio relationship between Vin and FB in LM27313 boost chip?
I have a 12V boost 24V power supply project on my side, currently I only see one in the specification book Δ VFB/ Δ The relationship between…
Part Number: LM27313
I am having an issue with the LM27313 Boost Converter. I have a circuit configured to match the typical application circuit illustrated in the datasheet. However, my output voltage is not stable when my load changes. I have the…
Part Number: LM27313-Q1 The input voltage is 3.3V and the output is about 12.5V. The current startup inrush current is about 1.1a. How to reduce the startup Inrush current below 900mA?
Part Number: LM27313 Hi Team,
When the input voltage of LM27313 is lower than 4V, the output voltage of LM27313 can be very stable, but when the input voltage is higher than 4V, you will see the voltage bounce, The input voltage of LM27313 should be…
Part Number: LM27313-Q1 Other Parts Discussed in Thread: LM27313 Hi,
I am using lm27313 for converting DC 12V to 24V. My initial load current will be 5mA. Is there chance of output voltage spike to 40V and come back to 24V?
Thanks.
Part Number: LM27313 Hello, Forum
Am I able to control the current value from the current source in the LM27313 ? If so, how?
I want to make it clear because there are some different constant values in the DATA Sheet, such as 5.5uA or 3uA as minimum…
Part Number: LM27313 Please tell me the formulae to calculate the power dissipation for LM27313XQMF/NOPB.
In the datasheet, the chapter 10.3 is only switching loss.I need also conduction loss,gate charge loss and supply current loss.
By the way, may…