Part Number: LM27313-Q1
Hi Team,
The LM27313XQMF is used to regulate 12V from Vin range from 5.6 to 6V.
TINA simulation shows dip in the output voltages regulation whereas in Webench there is no such Voltage dip for the load of 250mA.
Here are the circuit…
Part Number: LM27313-Q1 Other Parts Discussed in Thread: LM27313 Hi,
I am using lm27313 for converting DC 12V to 24V. My initial load current will be 5mA. Is there chance of output voltage spike to 40V and come back to 24V?
Thanks.
Part Number: LM27313-Q1 The input voltage is 3.3V and the output is about 12.5V. The current startup inrush current is about 1.1a. How to reduce the startup Inrush current below 900mA?
Part Number: LM27313-Q1 Other Parts Discussed in Thread: LM27313 , , LM2733 , LMR64010 , LM2731 , LM2735-Q1 , LMR62014 Hello,
Currently we are using LM27313-Q1 for boosting an input of 5V to 6.2V. We are planning to use LM2733XMFX/NOP & LMR64010XMFX/NOP as an…
Part Number: LM27313-Q1 Hi,
is it always necessary to use a 50kOhm resistor to pull up SHDN pin? What degrees of freedom do I have?
Thank you
Christian
Part Number: TPS62400-Q1 Other Parts Discussed in Thread: LP2998 , LM27313-Q1 , TPS62400 , HELLO TEAM
can you please offer the loop stability computation sheet of TPS62400、LM27313-Q1、LP2998?
Part Number: LM27313-Q1
5810.Power LM27313 (K-KdB).pdf
Hi all!
I have some trouble regarding to the LM27313-Q1.
I have implemented this circuit upon a project and it seems like the output is unstable, measuring with a scope gives me an unexpected sawtooth…
Part Number: LM27313-Q1 Other Parts Discussed in Thread: PMP10703 , LM2733
Hello all
I want to design power supply for gate driver IC of IGBT module (Three phase bridge).
So I want to use LM27313-Q1 to design flyback convertor which can output 15V(250mA) and…
Other Parts Discussed in Thread: LM27313-Q1 I would like to confirm the maximum duty cycle of LM27313-Q1.
In the datasheet, I found the minum value of maximum duty cycle 80%.
I have a question for this value.
When is the value 80% (high temperature or low…