Part Number: LM2735 I am having problems with the LM2735 components.
The boost output is not getting the output I want, it is much higher. And I think they are burning out the component. I need a 14V output, and I'm measuring voltages of 25-30V.
…
Part Number: LM2735 Other Parts Discussed in Thread: LM5088 ,
Hi,
We have a Li-Ion battery management system (BMS) running at 48V (nominal).
The input is driven through a DCDC (LM5088) to generate 5V, and then a LM2735 to produce 12.7V.
We have found that…
Part Number: LM2735-Q1 Other Parts Discussed in Thread: TPS61378-Q1 , LM2735 Tool/software: WEBENCH® Design Tools I want to know what would be the inrush current at the startup based on Webench report?
Attached below is the Webench report
7571.12V 120mA…
Part Number: LM2733 Other Parts Discussed in Thread: LM2735 Hello,
I have a question about LM2733.
I wonder how long will take time from input to output.
I can't find the information on spec. document.
Part Number: LM2735 Tool/software: WEBENCH® Design Tools I am using WEBENCH to create a circuit with LM2735 and I am not able to because the software always returns the error:
"Design cannot be created! Your preferred device does not work with the…
Part Number: LM2735 Hi Team,
Because this is a constant frequency converter, and I don't see pulse skip mode or PFM feature in datasheet, I'd like to make sure that this converter work in forced PWM in light load condition.
Thank you.
Best regards…
Part Number: LM2735 Tool/software: WEBENCH® Design Tools Hello,
i created a design in WeBench for the LM2735X with Vin in the range 3.7-4.2V and Vout = 5V @ 1.25A, and it gave me this schematic:
Even though in the datasheet a curve is not given for the…
Part Number: LM2735 Dear Specialists,
My customer is considering LM2735 and has a question.
I would be grateful if you could advise.
Could you please let me know the spec of frequency foldback at current limit.
I appreciate your great help in advance…
Hi Richard,
Apologize for the delayed response. We will take into account your feedback and update the alternate part selection dialogue to clarify that the values used are with DC-bias derated capacitance.
Regards,
Amod
Part Number: LM2735 Tool/software: WEBENCH® Design Tools My shared design webench.ti.com/.../SDP.cgi uses the default components now chosen by WEBENCH for the specified input and output requirements. The tabulated results show an output ripple voltage…