Part Number: LM2735 Tool/software: WEBENCH® Design Tools I'm seeing some odd behaviour in WEBENCH when I 'create a custom part' for Cout. This can be illustrated by comparison with Amod's shared design https://webench.ti.com/appinfo/webench…
Part Number: LM2735 Hi,
We intend using the LM2735y with an inductor having a secondary winding. The rectification takes place on the secondary winding in order to achieve a voltage of 200V. The leakage inductance on the primary side causes a short voltage…
Part Number: LM2735 Hello,
I want to use LM2735 in SEPIC configuration with :
Vout = 3.3V
3V < Vin < 5V
according to the datasheet, D/D' = Vout/Vin in SEPIC. Therefore : I out = I lpk * V in / (V in + V out ) if I neglect the ripple current
I lpk = 2…
Part Number: LM2735 Other Parts Discussed in Thread: LMR62421 , , LM3488 Hi,
I am looking for the cost effective solution in which input voltage is 3V to 4.5V and output is 3.3V
Here we have super capacitor at the input side
I saw LM2735 or LMR62421 sepic…
Part Number: LM2735 Other Parts Discussed in Thread: TPS61170 , TINA-TI Hello!
I've calculated component values for example circuits from LM2735 documentation to check the design equations before designing my converter.
8.2.12 LM2735X WSON SEPIC Design…
Other Parts Discussed in Thread: LM2735 Hello,
I know this is the wrong section but I want to learn about connection pins (J1, JR5, JR6, JR7) of LM2735 LLP/SOT TEST DEVELOPMENT TOOL designed by National semiconductor company. This company is under control…
Part Number: LM2735YSDEVAL Hello,
I want to learn about connection pins (J1, JR5, JR6, JR7) of LM2735 LLP/SOT TEST evaluation board. Because I could not find the datasheet of this board and the meaning of pins on it. I want to drive 2 inductive sensor…
Other Parts Discussed in Thread: LM2735 Hi,
In LM2735, I am generating 12V. Input Voltage +5V.
When I make Enable Pin = 0V. The output voltage is not completely going to '0V'. It is reducing from +12v to +4.9V.
I have connected a 100k Pull Up to…
Other Parts Discussed in Thread: LM2735 Hi all,
I have a question about how could we protect the LM2735 and its components L1 / D1 from a short circuit on the load side.
The circuit used is the typical one :
Vin = 5V
Vout = 12V,100mA
At the beginning …