Hello Matt,
EN will function with low impedance to VIN. There are two issues to watch for while laying out your design:
1. EN should not exceed VIN by 0.3 V. Since the LM2736 is a high performance part, keep the parasitic inductance between VIN…
Other Parts Discussed in Thread: LMR14206 , LM2736 Hello,
We have problem with a design with LMR14206.
Settings: Output 14.0V, Input from 18V to 28V.
With 150mA load everything is ok, but with no load and input 18.5V or lower the output is unstable.
…