Part Number: LM311-N Other Parts Discussed in Thread: LM311 , TLV1812-Q1 Hello guys,
One of my customers is considering using LM311M(X)/NOPB. They have the following questions. Could you please tell me your reply?
Q1. What is LM311-N minimum operation v…
Is the metal body of the voltage regulator LM337H/NOPB may cause the short circuit if it touches with other components/metal components? Because, from our understanding, the body of the component should be inductive, and not conductive. Can you please check…
Part Number: LM337-N-MIL In our Amplifier application, the Voltage regulator of LM337H/NOPB is touching the metal lid of the body casing, it then causes the failure: short circuit between this voltage regulator LM337H/NOPB and the lid body casing. It results…
Part Number: LM311-N Have been using Capture CIS 17.4 for a few months now and have been using components from the Cadence standard library. I've just started using Pspice for TI and I gather looking at other threads that trying to simulate a circuit…
Part Number: LM311 Other Parts Discussed in Thread: , LM6511 , LM211 Hi team,
What is the difference between LM311, LM311-N and LM311-M?
I can't see big difference between them on the internal circuit in the DS.
I would like to use it for GND standard…
Part Number: LM317-N-MIL
Hi Experts,
Good day. I am reaching out to guide us completing the information requested by a known Cx:
OPN
MIN INPUT
MAX INPUT
LM317K STEEL/NOPB
?
?
LM350K STEEL/NOPB
?
?
LM317HVK STEEL/NOPB
?
?
LM79L05ACM/NOPB
? …
Part Number: LM311-N Other Parts Discussed in Thread: LM393-N , LM311 , TL331 , LM339 , LM393 I'm using the LM311N/LM211P in a basic zero crossing detector circuit as in Fig 13. below with a pull-up voltage divider to give 3.3V logic output. The attached…
Kata-san
I moved the post to our High Rel group so they can assist. Even though it has a commercial temp range, it comes from the LM311-N-MIL family.
We reached out to their apps team offline as well so they are aware of the question.
Chuck
Hi,
?? ?? said: - allowing Number of vias
We recommend no more then 2 vias
?? ?? said: - allowed Length of via stubs
N/A. Try to minimize vias as much as possible. Typically go from top layer to bottom
?? ?? said: - maximum length limit
Depends on the insertion…
Hi Jimmy,
My mistake I used Ghz instead of Gbps.
It looks like with 157 ps/inch you are seeing 0.157 ps/mil and with an intra pair skew of 3.5ps that mean that if you divide the intra-pair skew we can see that 3.5/0.157 = 22.2 mils difference between…