Part Number: LM317M Hello everyone,
I am attempting to determine the maximum output current for the LM317M across a range of input and output voltages.
Section 6.5 Electrical Characteristics of the datasheet provides the following information:
However…
Part Number: LM317M Hi, Could you please explain the other conditions to understand Figure 6 & 10 below?
I calculated these data tables but I think this is not matched. how do I understand Figure 6 & 10?
Tj_ Max
125
℃
Am…
Part Number: LM317M Hi Support
Please help with below query regrading LM317M Design . attached Ref Circuit from datasheet.
Q1 ) How to decide R1 and R2 power rarting,
Q2) Can 0402 work on R1 and R2.
Q3) Image show R1 value 240 ohm, can we select higher…
Part Number: LM317M Other Parts Discussed in Thread: LM317-N , Hi,
In one of our projects we are using LM317-N for converting 27V to 5V @ 50mA, in field after running for sevaral months the regualtor is faling(getting short).
Input : 27V
Output: 5V
Current…
Hi Mahendra,
Unfortunately the KTP package is obsolete for the LM317M family. The thermal information does not appear to have been provided at anytime for the KTP package.
Very Respectfully,
Ryan
Part Number: SN6507-Q1 Other Parts Discussed in Thread: SN6507 , LM317 Dear Team,
We would like to have a feedback on our power stage for the SN6507DGQR .
Coul you please estimate the accuracy of the output? (our current estimation is ca. 25%) Also could…
Hi Philip,
I found that the RθJA value of LM317MKVURG3 is 56.9 °C/W.
You're correct -- this is not listed in LM317M's datasheet, but I was able to locate it on LM317's datasheet , on page 3. I will submit a request to add this information…
Part Number: LM317M Other Parts Discussed in Thread: LM317A , LM317L Dear TI engineer :
Can LM317M support constant-current Battery-Charger Circuit?
I fond LM317L and LM317A support constant-current Battery-Charger Circuit in datasheet, but I did not find…
Part Number: LM317M Other Parts Discussed in Thread: LM317 , My customer wnat to know ESD-HBM/ESD-CDM parameter for LM317,
but datasheet hasn't description,could you offer ESD-HBM/ESD-CDM parameter ? Thx