Part Number: LM336-2 Tool/software: There are 5 numbers next to the brand logo on the first line.
May i know what the meaning of the 5 numbers is?
Many thanks.
Part Number: LM336-2 Hi Experts ,
Can you please below DIE markings matches with the MPN : LM336BZ-2.5 to accept the parts.
Looking forward for your valuable support.
Regards
Manoj Balakrishnan.
Part Number: LM336-2 Hello,
We are using Lm336Z-2.5 , but currently the availability is a problem . As per the data sheet LM336BZ-2.5 seem to be same as Lm336Z-2.5. please confirm weather LM336BZ-2.5 can be used in place of LM336Z-2.5. also please let…
Part Number: LM336-2 I need a semi precise voltage and the LM336 looks like a good candidate. I need to amplify it to at least 5 volts and also gate it without affecting total output voltage. what op amp would you suggest to not corrupt output voltage…
Hi Cedrick
LT1004 and LM336 are shunt references (Similar to Zener diode ). You need to force a minimum current for a regulation.
A voltage source with a series resistor full fill that requirement. You can tune your resistor value based the the…
X1-1 provides 100 ohms at 0C and about 140 ohms at 100C. When I ran it the value was around 108 ohms. There is 1mV coming across Rref. X1-2 is used to measure resistance against to correct for distance errors (lines are the same length). The output at…