Part Number: LM3409HV we have requirement of suitable LED Drivers to drive 8A 20V led strings.
kindly suggest suitabel led drivers.
thanks ,
Nishanth C
Leuze electronics
India.
Part Number: LM3409HV Tool/software: Hi,
We are use the LM3409HV for the LED driver, the output current is 3.5A max.,
Now, the LED are turn on when the power on, and the LED will be turn off after 10mins, and we pull down the EN about 10s, the LEDs…
Part Number: LM3409HV Tool/software: Hello,
I am writing in order to have a clarification. Why does datasheet reports 5A as maximum current for load leds?
Since this is a buck controller i can choose external components with carachteristics compatible…
Part Number: LM3409HV-Q1 I am designing a high-power LED driver using the LM3409HVMY buck controller with a 12V DC input to drive a single LED (current target 2A, VF =1.8V). Despite several hardware adjustments, I am only seeing a few mA of output current…
Part Number: LM3409HV Hi All,
I'm currently building a led driver based on LM3409HV.
In my test I've seen that using 1uF (for test I'm using cheap electrolytic cap) on output will solve noise problems.
Which cap should I use? I'm looking for an…
Part Number: LM3409HV Other Parts Discussed in Thread: LM3409 , Tool/software: I am working on a design for an LED Driver using the LM3409HV. The input voltage is 48V and the board is required to drive different LED strings from 3.5A, to 4.5A maximum…
Part Number: LM3409HV Other Parts Discussed in Thread: TPS92641 , , LM3409 Hello Jonard,
we now have a 11 channel driver with components on both sides.
Please take a look to the pictures and both pdf attached.
I calculted all parameter with the…
Part Number: LM3409HV
Tool/software:
Hi TI Experts,
I have used LM3409HV to implement a 6A LED driver with shunt dimming feature Please note that the shunt dimming signal is not applied in the test stage so the output current is DC constant..
…
Part Number: LM3409HV Tool/software: Hi,
We use the LM3409HV for the LED Drivers, and now, we have below issue:
1. The circuit spec: The input voltage of LM3409HV is 40VDC, LED voltage is 32V, LED current is 3A, the inductance is 10uH;
Our issue…