Part Number: LM3411 Other Parts Discussed in Thread: TL431 Respected sir,
Can you provide any alternative Pspice model for the precision secondary regulator and driver just like LM3411.
Thanks & Regards,
N Srikanth.
Part Number: LM3411 Hi team,
Is there any FFF alternate for LM3411M5-5.0/NOPB, we have noticed that mentioned part is going to EOL.
Please specify the reason for EOL and when will the part becomes EOL.
Regards,
Rama Krishna.
Part Number: LM3411 Hi,
I am designing a push-pull converter whose output would be 120V, I want to use the LM3411 voltage reference with an optocoupler for the feedback. according to the datasheet, the LM3411 device only works for 3.3V and 5V. My question…
Part Number: TL103WB Other Parts Discussed in Thread: LM3411 I’m running into some issues with the TL103WB, I was wondering if you could have a look at my circuit. I’m getting around double the expected voltage (6.6V instead of 3.3V) out of the flyback…
Part Number: UCC28782 Other Parts Discussed in Thread: LM3411 Hi Team, Our customer intends to use UCC28782 to make a 5-10W wide input range, 5V output auxiliary power supply. In their case, no USB 3.0 PD controller is needed because they just want to…
Thanks for the details. This means you want to use "isolated" feedback.
For the schematic snippet you have shared, the COMP pin of LM5030 should be analyzed along with LM3411 internal circuit and the opto-coupler. There are two important things to note…
Hi Joe,
Thank you for this elaborate explanation. I noticed the problem of the different ON times of the two switches, it is actually a new development as they were equal when I first implemented the circuit, and the output voltage still dropped to…
Other Parts Discussed in Thread: LM2594 , LM3411 , TL431 Hello dear members, i am searching from few hours but unfortunately couldn't found a high previous voltage regulator ,i cam across LM2594 but it only supply 250mA and voltage is also not 5 volt…