Hi Frank,
Following up on the above. Is there a SPICE model for the LM36922H?
Also, an additional question can be seen below. Let me know if you need more info.
I am going to design with the LM36922H as the primary part, and use the LM36923H as the alternate…
Part Number: LM36922H Other Parts Discussed in Thread: LM36922 , , LM36923H Is there a dedicated EVM board with the LM36922H on it? Or is the LM36922 EVM the only development platform? Are the two part pin compatible and what are the differences?
Hi Rajesh,
You can set the sense resistor with 50mA, and decrease the PWM duty to 10% to get 5mA output. Yes, the current accuracy is related with the reference voltage accuracy.
For LM36923H,
1) This device supports paralleling channels.
2) It can also…
Part Number: LM36922H Other Parts Discussed in Thread: LM36923H , Please let us know 0x10 bit3 information.
There is not bit3 information in below table.