Part Number: LM3914 Tool/software: Do I need to leave the not connected pins on the LM3914 PLCC package (Pin 7 and Pin 9) open, or can I connect them to ground?
Part Number: LM3914 Other Parts Discussed in Thread: LP5009 , LP5012 Hi, I'm developing a circuit using the LM3914V/NOPB smt version. I've done some looking into inventory at a few suppliers and only found one vendor to have them in stock, only checked…
Part Number: LM3914 Other Parts Discussed in Thread: LP5009 , LP5012 Hi Experts,
Seeking your guidance please:
Is there a functional limit on how much the voltage on the outputs may exceed the supply voltage? From data sheet, I see an "absolute max. rating…
Hi,
Could you please provide me more information about the application of our customer?
Such as Bar or Dot mode?
I think the suggestion for them will depend on the scenario of usage.
Besides, LM3914 is a very old device, is it possible to suggest them…
Part Number: LM3914 I am using the example schematic for a zero to 4 Volt display. Pin 1 is always on faint even with the higher levels working pin 1 is always on. I replaced chip with 3915, 3916, and new 3914 but pin 1 in on dim.
My input is not floating…
Part Number: LM3914 Dear Sir,
Currently, I am using LM3914V with 25V Battery, it's working perfectly alright.
I am thinking to use LM3914V with a 48V Battery for level indication. Please let us know If there is any way to operate the IC safely with…
Part Number: LM3914 Other Parts Discussed in Thread: MM5452 , MM5453 , MM5483 , CD4054B Hi Team,
Our customer is using LM3914n-1 Bar/Dot LED and LCD Display Driver and is requesting a reference design (or any document) in which it is used to drive a character…
Part Number: LM3914 Dear Sir,
Currently I am using LM3914VX/NOPB for Battery level 18 V DC to 25.2 V DC.LM3914VX/NOPB does not support 3 LEDS or 4 LEDS Cell battery
I am looking battery Level Indication IC for 6 VDC to 8.4 VDC range with LEDs 3 or 4
…
Part Number: LM3914 Hello,
I like to make up a circuit using LM3914 with a 10 LED Bargraph to show the analogue voltage being generated by a RF power detector. The voltage range is 0 to 3.2V.
Does TI have a PCB breakout of LM3914 with 10 LED Bar graph…
Part Number: LM3914 Hello,
Thank you for answering to my question regarding the replacement part for LM3914 in DIP version.
I will look into PLCC package form as you requested. However, there are two versions and I am not sure what are the differences…