Part Number: LM4132 Hi Expert,
Whether LM4132 NC pin can be connected to GND?
In datasheet, it is said "floating", but for compatible design, we need to connect GND to NC pin.
Does this have any problem?
Thanks.
Zhou
Part Number: LM4132
Hi,
We are using this IC in our product. in production our board will not be power on externally and we will program the board with programmer supply. in this programming time the reference IC verf pin will get 1.8V (because of programmer…
Part Number: LM4132-Q1 Other Parts Discussed in Thread: LM4132 Dear Team,
I have a specific question regarding LM4132CQ1MFR3.0. In a design we can not always guarantee the LM4132 is supplied correctly or supplied at all, whereas the rest of the circuit might…
Part Number: LM4132 Hi,
We are looking for Load Independent constant current source, Load current value will be 5mA. Load resistance will vary from 650 Ohm to 850 Ohm. Input power is 5V.
Also, it should have lower temperature coefficient, because this…
Part Number: LM334 Other Parts Discussed in Thread: LM4030 , LM4132 Hi,
We are looking for Load Independent constant current source, Load current value will be 5mA. Load resistance will vary from 650 Ohm to 850 Ohm. Input power is 5V.
Also, it should have…
Other Parts Discussed in Thread: LM4132 Hello Team ,
i am using the LM4132 - 4.096 in one of a high precision design as a reference to a 16 bit DAC
I wanted to know if there was any way i could reduce the output 1/f noise to less that the 1 - LSB of my…
Other Parts Discussed in Thread: LM4132 , ALLIGATOR Hi, I'm currently trying to design the passives around an LM4132 2048mV ref, so far I have: 3v input (coincell 2032) 10uF + 100nF on input 100nF on output Loaded with a 2Kohm resistor All the components…
Other Parts Discussed in Thread: LM4132 Hello. I am reviewing a circuit in which the LM4132BMF-3.0/NOPB 3 Volt reference has been used with a larger output capacitor than input capacitor. The datasheet is explicit that this is not allowed:
The value of…
Other Parts Discussed in Thread: LM4132-Q1 , LM4132 , REF5025 Dear, All
The customer is considering the LM4132-Q1. They are focused on Long-Term Stability. However, the data sheet of LM4132-Q1 is not listed is Long-Term Stability. Please provide if there is…
Thank you for sharing information.
Actually, t here will be an inrush current as soon as the sampling switch is turned on to charge the sampling capacitor. Here LM4132 is used for VREFHI, in which the output current is not supplied by an internal buffer…